Hi,
Do you have a behavior model of AD9581?
I would like to simulate a behavior of AD9851.
If there are any test bench, can you provide me?
Best regards,
Tsurita
AD9851
Production
The AD9851 is a highly integrated device that uses advanced
DDS technology, coupled with an internal high-speed, high
performance D/A converter, and comparator...
Datasheet
AD9851 on Analog.com
Hi,
Do you have a behavior model of AD9581?
I would like to simulate a behavior of AD9851.
If there are any test bench, can you provide me?
Best regards,
Tsurita
Hi MakotoTsurita ,
Are you referring to an IBIS model? If so, apologies but we currently do not have one for AD9851. Although AD9850 has one but I could not confirm whether they're compatible to your application, but I can see that AD9850 and AD9851 have differences in terms of sample rate, maximum Iout, AD9850 has integrated PLL, and differences in power consumption. So, I think it is safe to say that they're not compatible.
However, if you really need it, you can contact your local Field Application Engineer and have it requested for you.
All the best,
Jules