Post Go back to editing

Need single Frequency Output with higher current drive

Category: Hardware
Product Number: AD5933

Hi,

I have an application where I want to tune the Vpp (peak to peak voltage) and Vdc (dc voltage) of a sinusoidal output waveform. The AD5933 IC does exactly that but my application does not demand a frequency sweep. I want to generate a fixed configurable frequency. How can I do that using AD5933? I am with the idea that it's not possible to do it but still wanting to know if I am missing certain configuration settings.

Also, my application demands output current in the range of 40mA - 100mA and therefore I am looking for a "High Current DDS". Can someone suggest me the exact IC part number that can satisfy both of my requirements?

Regards,

Chetan.