Post Go back to editing

Ad9914 Eval Board Device Control via TCP/IP

Category: Software
Product Number: AD9914

Hello,

I am looking to see if there is a recommended route for sending commands to the microcontroller of the AD9914 Eval board via TCP/IP from the host PC which is then converted to USB/serial via an ethernet to USB converter.  In the past, we have controlled this device with direct USB connection and utilizing python/WinDLL to load in the adiddseval.dll to send commands.  I was wondering if there is a recommended approach for the above communication setup?

We have also considered bypassing the microcontroller and directly communicating with the board via serial, which is the approach we may take if there is no route recommended for the ethernet to usb communication setup.

Thanks in advance!



title edit
[edited by: cfol at 8:20 PM (GMT -4) on 6 Jun 2024]

Thread Notes

Parents Reply Children