Post Go back to editing

Arduino connect with AD 5933 , Turn ON issue, push pull resistors

Category: Hardware
Product Number: AD 5933 evaluation board

Dear Members
Hope you are fine
I have a few questions
1) I have connected a 3.3V GPIO pin with the VDD of the EVAL AD 5933 evaluation board using jumper wire and ground with the ground. But the EVAL AD 5933 evaluation board does not turn ON ( Indication: check the EVAL AD 5933 evaluation board power LED, it remains OFF)
why my EVAL AD 5933 evaluation board doesn't turn ON although in the forum many people said it turns ON with 3.3V of Arduino.

2) I have soldered wires on R15 and R16 pins on the AD 5933 evaluation board for I2C communication purpose and connected them with A4 and A5 pins on Arduino respectively.
does there is a need for a push-pull resistor for I2C communication or not?

3) Could I control all the parameters through Arduino coding? Parameters like Vpp, calibration impedance, PGA control, DDS setting time, and calibration gain factor or I have to first connect my EVAL AD 5933 evaluation board with my computer and adjust the parameters using the company-provided software and then I turn OFF the software( detach the power cable) and then connect with the Arduino to avil the required changed parameters,( again give power using 3.3V of Arduino UNO)

If anyone has these answers, kindly let me know.
Thanks in advance all of you.