Category: Hardware
Product Number: ad9914
Software Version: ise14.7
Hi, We are using AD9914 in our board. After power up, we need to see the SYNC_CLK output at the pin 82,we use the the oscilloscope to see it ,whe the temperature is 25℃,its power is 1.8V。whe the temperature is 0℃,its power is 2.2V。Dose the power of the SYNC_CLK change with the temperature?I can not see the description of power of SYNC_CLK description in the datasheet。