I am using the AD9958 to conduct a continuous linear sweep, creating essentially a triangle wave from S0 to E0 and switching right at the start and end frequencies.
My question is what is the delay between the profile pin changing and the sweep changing directions/beginning? The datasheet mentions that the maximum toggle rate for the profile pins is 2 sync clk cycles, but doesn't mention what the internal delay for the sweep to begin is
I am feeding a 100MHz clock to the part and multiplying it up by 5 to get a 500MHz state machine clock and a 125MHz sync clock