Post Go back to editing

AD9951 Amplitude

Dear Technical Support Team,

Hi,

My circuit shows 290mVpp on 50Ω pullup and 550mVpp Single-End through transformer.

Settings of AD9951 are 10mA(FullScale with ASF=0x3FFF) and 12.88MHz 

Is it expected amplitude?

Here is schematic and waveform.

PDF

It seems that there is a resistance of about 50Ω in parallel on the secondary side of the transformer.
When the impedance on the secondary side reaches about 38Ω,

Primary side: 275 mVpp
Secondary side: 550 mVpp

It will be about.
If there is about 50Ω in parallel on the secondary side

50Ω // (51Ω + 49.9Ω + α) = 38Ω
α is the impedance of the LC filter (at 12.88MHz)

Best Regards,

ttd

Parents Reply Children