Post Go back to editing

AD9910: DROVER pin active bit?

Hi,

I want to use the (ad9910) DRG in normal ramp generation, in the page number 29 of data sheet it states:" In Figure 39, a sample ramp waveform is depicted with the required control signals. The top trace is the DRG output. The next trace down is the status of the DROVER output pin (assuming that the DROVER pin active bit is set). The remaining traces are control bits and control pins."

I could not find such a register bit that I could configure. 

Is there a such DROVER pin active bit available? Could you please clarify.

Thanks & Regards,

Gautam.



updated Tags
[edited by: gautamtada at 10:05 AM (GMT -4) on 28 Jun 2021]
Parents Reply Children
No Data