Post Go back to editing

EVAL-AD9954

Dear Technical Support Team,

Could you provide user guide of EVAL-AD9954?

analog.com/jp/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-ad9954.html

Best Regards,

ttd

Parents
  • Hi,

    Unfortunately, there is no published user guide for the EVAL-AD9954 but you can use the attached document as a user guide.

    DOC

    Best regards,

    Mark

  • Hi Mark,

    Thank you!

    I have three questions about EVAL-AD9954

    1.)

    According to the user guide REF CLK should be 400MHz. AD9951 has internal multiplier. 

    Is it possible to use 100MHz with x4 multiplier?

    2.)

    0dBm means 0.632Vpp(50Ω)?

    ------------------

    Connect SMA to REF CLK DUT1 (J3) port. The signal source output frequency should be 400 MHz and a power output of 0 dBm. The clock signal input should only appear at the REF CLK DUT1 when the AD9954 Evaluation Board is fully powered up.

    ------------------

    3.)

    Is it possible to use USB to parallel Printer Cable?

    Best Regards,

    ttd

Reply
  • Hi Mark,

    Thank you!

    I have three questions about EVAL-AD9954

    1.)

    According to the user guide REF CLK should be 400MHz. AD9951 has internal multiplier. 

    Is it possible to use 100MHz with x4 multiplier?

    2.)

    0dBm means 0.632Vpp(50Ω)?

    ------------------

    Connect SMA to REF CLK DUT1 (J3) port. The signal source output frequency should be 400 MHz and a power output of 0 dBm. The clock signal input should only appear at the REF CLK DUT1 when the AD9954 Evaluation Board is fully powered up.

    ------------------

    3.)

    Is it possible to use USB to parallel Printer Cable?

    Best Regards,

    ttd

Children