AD9854 - Arduino interfacing

Hello,

I developed a circuit board with AD9854 to generate a frequency sweep from 10MHz to 100MHz. The circuit board should work in one wave-mode (sine or cosine wave, I don't need a quadrature signal). I would like to use an arduino-based board to control the AD9854. I am wondering if the Arduino Due can be the right choice (since it has native 3.3V I/O Ports) and if you can provide me some libraries or example codes for this purpose.

Thank you for supporting!

Best,

Simone