AD9834
Production
The AD9834 is a 75 MHz low power DDS device capable of producing high performance sine and triangular outputs. It also has an on-board comparator that...
Datasheet
AD9834 on Analog.com
Hi Everyone,
I am using the AD9834CRUZ DDS chip with a 75MHz MCLK (all on an arduino shield). The chip is being programmed by an Arduino Duemilanove. I want to use it to ultimately produce a signal in the 27MHz band but currently am having trouble even getting just a 1kHz output.
What happens during testing is that when the AD9834CRUZ is powered up I instantly get a signal at the output of 2.65MHz even though I have not programmed the registers and also regardless of what frequency I even set the registers to. I decided to build another board and the same result occurs with a constant ouput of 2.65kHz regardless of frequency register.
I suspected the MCLK initially until I managed to achieve 37.5MHz output at one point but that was due to a noisy SDATA and SCLK line which has since been fixed.
Below are schematics and coding for a basic test of the AD9834CRUZ for an output of 1kHz.
Kindest Regards,
TL
/*
Code for programming one frequency of the AD9834.
*/
// Global Variables
int ChannelTransmit = 0;
int Done = 0;
int FreqReg0[]= {0,1,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,1,0,0,0,0,1,1,0,1,1,1,1,1,1,1,0,0}; //1 kHz
int ContReg[] = {0,0,1,0,0,0,0,1,0,0,0,0,0,0,0,0};
int ResetReg[] ={0,0,1,0,0,0,0,0,0,0,0,0,0,0,0,0};
int PhaseReg0[] = {1,1,0,0,0,0,0,0,0,0,0,0,0,0,0,0};
int FSELECT = 8; // FSELECT pin of the AD9834CRUZ.
int RESET = 9; // RESET pin of the AD9834CRUZ.
int SDATA = 10; // SDATA pin of the AD9834CRUZ.
int SCLK = 11; // SCLK pin of the AD9834CRUZ.
int FSYNC = 12; // FSYNC pin of the AD9834CRUZ.
void setup()
{
for(int pin = 1; pin < 9; pin++)
{
pinMode(pin,INPUT); // Sets the AD9834CRUZ pins.
}
for(int pin = 8; pin < 13; pin++)
{
pinMode(pin,OUTPUT); // Sets the AD9834CRUZ pins.
}
digitalWrite(FSYNC, HIGH);
digitalWrite(RESET, HIGH);
digitalWrite(FSELECT, LOW);
digitalWrite(SCLK,HIGH);
}
void loop()
{
ChannelTransmit = digitalRead(3);
if(ChannelTransmit == LOW)
{
Done = 0;
}
if(ChannelTransmit == HIGH && Done == 0)
{
Done = 1;
digitalWrite(SCLK,HIGH);
digitalWrite(FSYNC,LOW);
for (int i = 0; i <= 15; i++)
{
digitalWrite(SCLK,HIGH);
digitalWrite(SDATA,ContReg[i]);
delay(10);
digitalWrite(SCLK,LOW);
delay(10);
}
FSYNCsetup();
for (int i = 16; i <= 31; i++)
{
digitalWrite(SCLK,HIGH);
digitalWrite(SDATA,FreqReg0[i]);
delay(10);
digitalWrite(SCLK,LOW);
delay(10);
}
FSYNCsetup();
for (int i = 0; i <= 15; i++)
{
digitalWrite(SCLK,HIGH);
digitalWrite(SDATA,FreqReg0[i]);
delay(10);
digitalWrite(SCLK,LOW);
delay(10);
}
FSYNCsetup();
for (int i = 0; i <= 15; i++)
{
digitalWrite(SCLK,HIGH);
digitalWrite(SDATA,PhaseReg0[i]);
delay(10);
digitalWrite(SCLK,LOW);
delay(10);
}
FSYNCsetup();
for (int i = 0; i <= 15; i++)
{
digitalWrite(SCLK,HIGH);
digitalWrite(SDATA,ResetReg[i]);
delay(10);
digitalWrite(SCLK,LOW);
delay(10);
}
digitalWrite(SCLK,HIGH);
digitalWrite(FSYNC,HIGH);
delay(10);
digitalWrite(SCLK,LOW);
delay(10);
digitalWrite(SCLK,HIGH);
digitalWrite(RESET,LOW);
}
}
void FSYNCsetup()
{
digitalWrite(SCLK,HIGH);
digitalWrite(FSYNC,HIGH);
delay(10);
digitalWrite(SCLK,LOW);
delay(10);
digitalWrite(SCLK,HIGH);
digitalWrite(FSYNC,LOW);
delay(10);
digitalWrite(SCLK,LOW);
delay(10);
}
Hi,
Schematic looks OK from first impressions.
Please refer to AN-1070 for initialisation sequence. Do you see that the correct data is loaded on the SPI bus ?
-liam
Hi Liam,
Thanks for you reply.
Yes I have checked the data loaded onto the SPI bus using a logic analyzer and the data is being loaded correctly. The initialization sequence is also carried out according to the AN-1070 application note.
Attached is a screenshot of this, although this was on an occasion where different data was being loaded onto the board the data was cross-checked with data in the code used and the same initialization sequence format was used being: controlregister->14LSB fregister0 -> 14MSB fregister0->controlregister->14LSB fregister1 -> 14MSB fregister1->pregister0->pregister1->resetoff.
Can you have a look at Serial bus with an oscilloscope - make sure the correct data is there. Make sure the timing is correct etc.
Also can you check if the part actually goes into reset when you send a RESET command.
-Liam
I am controlling reset using the reset bit; How do I check if the part has gone into reset?
EDIT: sorry I am using the control pins
In addition to this, I have tested the AD9834 with no inputs to the programming pins and I can still get an output of 2.65MHz, this seem strange as the datasheet says that on power up the registers are loaded with invalid data.
Hi,
I missed the last post on this thread apologies. Are you still having issues here ?
-Liam