I need fine drive output amplitude at AD9954.
My question is. Is possible use anything as http://www.analog.com/static/imported-files/circuit_notes/CN0156.pdf ?
If so within what limits can control the amplitude?
AD9954
Production
The AD9954 is a direct digital synthesizer (DDS) that uses advanced technology, coupled with an internal high speed, high performance DAC to form a complete...
Datasheet
AD9954 on Analog.com
I need fine drive output amplitude at AD9954.
My question is. Is possible use anything as http://www.analog.com/static/imported-files/circuit_notes/CN0156.pdf ?
If so within what limits can control the amplitude?
The AD9954 is equipped with output amplidtude control. Have you considered using the internal output scalar to control output amplitude? If not, then enable the OSK enable bit in register CFR1 bit <25> and then use the Amplitude Scale Factor register (ASF) 0x02 and you'll have 14-bits of amplitude resolution.
Hi. I know this is a very old thread but i want to use ASF for AD9954 single tone mode operation. As you mentioned I need to set OSK enable bit and write to ASF register but what should be the state of the OSK physical pin? high or low? I want to use ASF register for amplitude control of single tones generated. thanks
Hi. I know this is a very old thread but i want to use ASF for AD9954 single tone mode operation. As you mentioned I need to set OSK enable bit and write to ASF register but what should be the state of the OSK physical pin? high or low? I want to use ASF register for amplitude control of single tones generated. thanks