Post Go back to editing

AD9914 heat dissipation (eval board)

Hi,

I noticed that the integrated circuit on the AD9914 evaluation board gets rather hot. Should there not be a heat sink mounted on it?

Enabled mode

3.3 V rail @ 610 mA

1.8 V rail @ 83 mA

Power down mode:

3.3 V rail @ 164 mA

1.8 V rail @ 26 mA

Parents Reply Children