Post Go back to editing

AD9838 - Jittering at Some Frequencies

     Good morning.  My customer wants to use the AD9838 DDS and is currently evaluating the part via the evaluation board.  His frequency range of operation is 40KHz up to 1MHz in 256 steps of 3.750KHz.  He has the IOUT pin going into the VIN pin as it is on the demo board using an RC filter composed by 300W resistor and a 0.1mF capacitor.  The calculated cut frequency for this filter is FC=5.3KHz.  The circuit is working and I get the square wave desired.  The only problem is the jittering in some frequencies on my scale.

     Question:  I'm planning to implement a 3-pole RC filter coming from IOUT to Vin to see if I can reduce jittering.  Which cut frequency do I need to have on my filter?  I have read the AN-837 talking about the filter, but a 7th order elliptical filter I feel is unnecessary.

 

Parents
  • Ok,

    We will live with that. The result of the DDS is to generate a specific frequency to be used for a 8th order lowpass eliptic filter MAX7404. The signal will not be affected by this jitter. I just would like to improve the max i could to keep project clean. But that's fine. If we decided eventually to improve we will sub the microcontroller signal with a crystal class B as you mention with 15975MHz.We can close this case. thanks for support.

Reply
  • Ok,

    We will live with that. The result of the DDS is to generate a specific frequency to be used for a 8th order lowpass eliptic filter MAX7404. The signal will not be affected by this jitter. I just would like to improve the max i could to keep project clean. But that's fine. If we decided eventually to improve we will sub the microcontroller signal with a crystal class B as you mention with 15975MHz.We can close this case. thanks for support.

Children
No Data