How to measure the impedance charactersistics of a unknown valued resistor or capacitor using AD5933  ? Please help friends

Hi Friends,

I am stuck with my project. I have to measure the frequency characteristics of an unknown impedance valued sensor.

How to do that ?

Parents
  • Hi.

    Apologies for the delay. I have overlooked your follow-up question.

    The board should always be calibrated for a change in any of the following parameters:

    • Current-to-voltage gain setting resistor
    • Output excitation voltage
    • PGA gain

    The board is calibrated again because there would be a change in the gain factor when any of the above mentioned parameters is changed.

    The Rfb is used so that the ADC will not be saturated.

    We tried to measure an unknown capacitance by using 150k for Rfb and 210k for Rcal. The same procedure for calibration that was done in measuring an unknown resistance was used.

    Then the capacitor was placed on Z and the Start Sweep button was pressed. This is what we obtained:

    Magnitude:

    Phase:

    You can download impedance data and compute the capacitance by using the formula:

    Xc = 1/(2*pi*f*C)

    From the impedance data, we chose a frequency of 30 kHz and an impedance of 342765.3. We obtained a capacitance value of 15.48pF.

    Hope that helps.

    -Sittie

  • Hi,

    I've just started using the
    EVAL-AD5933EBZ and really looking for a how-to guide.
    I'm not finding the official users guide (UG-364) comprehensive for beginner like me and have a few basic questions that is not explicitly answered (or at least I failed to find it)

    1) The "Calibration Impedance" in GUI (v1.5) corresponds to which physical element in the development/evaluation board ?

    Calibration Impedance

    2) The Vin/Vout referred in the following corresponds to what in EVAL board ?


    as according to the schematic shown below
    Rfb

    It is appears to be "RFB" is Calibration Impedance (ref. GUI) as I failed to find Rcal in schematic extracted from UG-364
     or any element on EVAL Board marked as Rcal/RCAL.

    If Rcal is Rfb, where to place the unknown impedance that I want to find out, in the element "Z" of the EVAL board, or between "T7 and T8" as it is across Vin and Vout, as stated in GUI manual.

Reply
  • Hi,

    I've just started using the
    EVAL-AD5933EBZ and really looking for a how-to guide.
    I'm not finding the official users guide (UG-364) comprehensive for beginner like me and have a few basic questions that is not explicitly answered (or at least I failed to find it)

    1) The "Calibration Impedance" in GUI (v1.5) corresponds to which physical element in the development/evaluation board ?

    Calibration Impedance

    2) The Vin/Vout referred in the following corresponds to what in EVAL board ?


    as according to the schematic shown below
    Rfb

    It is appears to be "RFB" is Calibration Impedance (ref. GUI) as I failed to find Rcal in schematic extracted from UG-364
     or any element on EVAL Board marked as Rcal/RCAL.

    If Rcal is Rfb, where to place the unknown impedance that I want to find out, in the element "Z" of the EVAL board, or between "T7 and T8" as it is across Vin and Vout, as stated in GUI manual.

Children