Post Go back to editing

generating high frequency triangle wave using AD9834

hi all,

i'm new to this forum and also to DDS application..

so i have a task to create a triangle wave with frequency of 36MHz..

is it possible to do this task using AD9834 chip?

i wonder that the update rate of AD9834 is only 75MSPS , is it possible to create a good triangle at my required frequency..

thank you very much

regards,

franz

  • Hi Frans,

    I don't think it would still look like a triangle if we push the waveform's fundamental frequency at 36 MHz because it is very near to the nyquist frequency. It is best to let at least the 5th harmonic of the waveform to be less than the nyquist frequency in order to get a proper looking triangular wave. Having that, it would only be around 7 MHz of frequency.

    Best Regards

    Louijie

  • hi LouijieC,

    thanks for your respond..

    do you have any recommendation of DDS chip which can create a triangle/sawtooth wave at frequency 36MHz?

    to accomplished the 5th harmonics, i think that the sampling rate should be more than 360MHz..

    in that case, can i use AD9953 (400MSPS) to generate triangle waveform?

    thank you

    Best regards,

    frans

  • Frans - All of the DDS parts we have running at >100MSPS rely on an angle to amplitude algorithm which doesn't allow us to directly implement anything other than a sinusoid.  That said, it is possible to fake the DDS out a little if it has amplitude sweep capability by setting the a phase offset word so that the DDS engine is stuck at 90 degree (assuming it's doing a sin(x) function), then performing amplitude sweeps.  Note, though, that you lose some of the functionality (phase tuning, e.g.) with this approach.

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin