AD9913 REF_CLK to O/P LATENCY

I'd like to use an AD9913 DDS in a phase sensitive application where the typical set-up is REF_CLK input is 49.805 MHz, and the DAC O/P is 49.8025 MHz. The PLL multiplier is set to 5. When first activated, there will will be some specific latency between the REF_CLK I/P and the DAC O/P. If the REF_CLK I/P is interrupted for several seconds, when the signal is restored (no frequency changes) is there a process by which I can ensure that the latency is the same as originally measured? I'm assuming that this is not the same as the Data Latency figures?

Thank you

Bob

Parents Reply Children
No Data