AD5933
Production
The AD5933 is a high precision impedance converter system solution that combines an on-board frequency generator with a 12-bit, 1 MSPS, analog-to-digital...
Datasheet
AD5933 on Analog.com
1.Please suggest the circuit diagram for 4-electrode configuration for human body thoracic impedance measurement range 0-60 ohm using ad5933
2.I want inject ac current 200uA at 100khz ...please suggest the Resistor and capacitor value in the circuit diagram
3.Two electrodes for injecting the current and another two electrodes for sensing the voltage
4.I want operate the circuit at single power supply
5.I have referred the link: AD5933 4 Wire Configuration for low impedence (< 50 ohm) but there is no clarity in the diagram.Please suggest the circuit diagram for 4-electrode configuration for human body thoracic impedance measurement range
Hi Sanjay,
I do not think you can measure thoracic impedance and perform ECG measurements simultaneously since the current source from the impedance measuring circuit will act as a source of disturbance to the ECG circuitry which might explain why ECG waveform characteristics are not seen.
We advise you to consider taking a look at ADAS1000 as front end ECG and for thoracic impedance measurement.
Cheers,
Ivan
Hi Sanjay,
I do not think you can measure thoracic impedance and perform ECG measurements simultaneously since the current source from the impedance measuring circuit will act as a source of disturbance to the ECG circuitry which might explain why ECG waveform characteristics are not seen.
We advise you to consider taking a look at ADAS1000 as front end ECG and for thoracic impedance measurement.
Cheers,
Ivan