ad9913 super nyquist operation

Hello, I want to use the AD9913 DDS for super nyquist operation. I don't need very high signal levels or particularly great phase noise. Maybe a signal down as low as -40 or -50 dBm would be ok. Given that, is there any problem trying to extract the 58th image? The Fref would be 100 MHz, and assuming no multiplier, I would like to be able to target ~2940 MHz. Thank you.

Parents Reply
  • 0
    •  Analog Employees 
    on May 18, 2020 12:29 PM 8 months ago in reply to gwongLL

    I don't currently have access to an Eval. Bd., so I am unable to do a quick check. Beside, as you note, the sinc response is only part of the story as there are the package and PCB parasitics to consider, as well. So, even with setting up an Eval. Bd., there would be losses associated with the PCB and external components that were not given design consideration for >2 GHz operation.

Children
No Data