AD9914 DAC calibration

Hello: ADI technical engineer.           

Excuse me: the DAC calibration of ad9914 mainly corrects those functions of the chip.           

How long is the best time for DAC calibration after power on, and how long is the internal program loading of ad9914.           

The usage is as follows:           

1. The reference clock of DDS is 3.5GHz;           

2. DAC calibration shall be carried out 0.5ms after FPGA program runs normally;           

3. DAC output always switches between 720MHz and 720MHz + 500Hz.           

The fault phenomenon is as follows:           

1. After power on, 720MHz ± 8.9khz spurious is good or bad, sometimes 72dbc, sometimes 47dbc.           

2. When the frequency of 100MHz constant temperature crystal is doubled to 3.5GHz and the signal source (R & s ® sma100b) provides 3.5GHz, the above strip phenomenon will occur (because the frequency stability of constant temperature crystal is poor when it is powered on, two methods are used for testing).           

3. The test picture is as follows  

          

4. The modification is as follows           

  • ①  after the FPGA program runs normally, calibrate the DAC within 5ms;           

3.5GHz from 100MHz constant temperature crystal oscillator frequency doubling           

The fault phenomenon is as follows:           

72 DBC for 720MHz ± 8.9khz, but 25 DBC for 1K, 17 DBC for 10K, and 10 DBC for 10K,           

The test picture is as follows

Parents Reply Children
No Data