EVAL-AD5933 Basic Impedance Measurements

Hi,


I got today my EVAL-AD5933EBZ board and have some issues with the first measurements. I followed the instructions in the guide of the EVAL board, but getting some strange results. Maybe I misunderstood some parts in the guide.


After installing the software (downloaded from the internet), I checked the configuration of the jumpers. Following configuration is active on the board:


LK1 = open, LK2 = open, LK3 = closed, LK4 = open, LK5 = closed, LK6 = A


To perform the first frequency sweep of 30 kHz to 32 kHz across a 200 kOhm resistor, I put in the sockets of RFB (left of R2 and above R4) a 200 kOhm resistor as feedback resistor. Additionally I connected the "unknown" 200 kOhm resistor to the Z sockets left of the place for C2.


I configured the parameters in the software and programmed the device registers. Then I performed a gain factor calibration by pressing "Calculate Gain Factor" and got 5.11035456561638e-10, which is similar to the value of the screenshot in the manual.


When starting a sweep I got following impedance curve:


When now replacing the "unknown" 200 kOhm by a 100 kOhm resistor, I get following results. Yes, RFB is still 200 kOhm.

The results is nearly the half of the first measurement, which I expect. But in both measurement I got a wrong exponent. Did I do something wrong during calibration? Is it software issue with Windows 7?

Thanks in advance.

-Christoph

Parents
  • You seem to do everything right, but with your settings setting you cannot measure resistors smaller than Rfb installed on the board, which is likely 200k. Your calibration is probably OK as your Rcal=Rfb. I would try measuring larger resistors, say, 220k, 250k, 300k, etc.and see how those values come out. 

Reply
  • You seem to do everything right, but with your settings setting you cannot measure resistors smaller than Rfb installed on the board, which is likely 200k. Your calibration is probably OK as your Rcal=Rfb. I would try measuring larger resistors, say, 220k, 250k, 300k, etc.and see how those values come out. 

Children