Hi,
I am trying to use about a 9 year old AD9910 Eval Board to generate a range of sine waves say upto 400Mhz.
Unfortunately, I feel there are issues with it. There is an output- though but it appears distorted and I am unable to get it locked.
The signal appears to be like a frequency modulated wave even if I am using this in the normal mode.
Checking the signal at the SYNC-CLK (J9) also one sees a similar waveform. This is puzzling.
Earlier when i was using Windows XP, it had worked well. But now I have upgraded to windows 7 pro version- 32 bit.
Would this be the cause of the misbehaviour?
or what could be the problem????
Thanks in advance.
Thanks Ken.
I have reinstalled it. I have the older version 1.0 of the software. Even after reinsatllation the output is the same.
I tried to install the new version 2.1.0; but with this, the software…
You can just install version 2.1.0 which should uninstall version 1.0 for you.
On power up the USB Controller (U7) reads the board identity from the EEPROM (U3).
If W3 is not installed on power up, the USB…
Hi Shane,
Did as directed. uninstalled the previous version and installed the 2.1.0 from the AD website.
Downloaded and installed the USB EB programmer as per directed.
However I find the below message popping up :
Device driver Software was not successfully installed
Cypress EZ-USB FX2 (68613) - EEPROM missing √ Ready to use
Unidentified Device × Device Unplugged
ADI Evaluation system (LRFDev) √ Ready to use
Kindly advice. Thanks
Also the CR 2 is flashing and the left bottom of the Evaluation Software it shows that 'Not Connected" also flashing in Red. Next to this it shows AD9910.
Secondly, during the initial running of the software, it shows the RED window.
Please reply.
Thanks
Hi pra-kash, Please you verify the following information on your PC.
1) Open device manager, the evaluation board should be listed in device manager as shown in the following screenshot.
If it is not try powering your PC and evaluation board off and back on. Then try the software again. If it still won't connect please let me know how the evaluation board is displayed in device manager with Hardware Ids.
2) The start screen for the AD9910 Evaluation Software should look like the following screen shot, and should display Version 2.1.0.
Thanks Shane for your prompt reply.
The computer shows exactly as you have shown on your above reply.
Also, I tried powering the board ON -OFF and connecting -disconnecting the USB connection to the PC. The CR2 LED is flashing @ ~1 per sec and on running the Evaluation software it shows exactly as you shown but the STATUS is in RED.