Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      World Engineering Day Quiz!

      By Kuo-Chang A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

EngineerZone
EngineerZone
Data Converters
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Data Converters
Data Converters
Documents What are the recommended values of C1 in the MAX31865 typical application circuit?
  • Files
  • FAQs/Docs
  • Members
  • Sub-Groups
  • Tags
  • Cancel

Products Mentioned

MAX31865 Production
The MAX31865 is an easy-to-use resistance-to-digital converter optimized for platinum resistance temperature detectors (RTDs). An external resistor sets...
Datasheet
MAX31865 on Analog.com

Table of Contents
  • DATA CONVERTERS SUPPORT COMMUNITY
  • +Documents (More FAQs in Sub-Groups)
  • +AD7730: FAQ
  • +AD7746: FAQ
  • +ADC: FAQ
  • +AD1871: FAQ
  • +AD1877: FAQ
  • +AD1974: FAQ
  • +AD2S1200: FAQ
  • +AD2S1205: FAQ
  • +AD2S1210: FAQ
  • +AD2S80A: FAQ
  • +AD2S83: FAQ
  • +AD2S90: FAQ
  • +AD4080: FAQ
  • +AD4081: FAQ
  • +AD4083: FAQ
  • +AD4084: FAQ
  • +AD4086: FAQ
  • +AD4087: FAQ
  • +AD4880: FAQ
  • +AD4883: FAQ
  • +AD4884: FAQ
  • +AD5111: FAQ
  • +AD5112: FAQ
  • +AD5115: FAQ
  • +AD5116: FAQ
  • +AD5121: FAQ
  • +AD5141: FAQ
  • +AD5141BCPZ100-RL7: FAQ
  • +AD5142: FAQ
  • +AD5160: FAQ
  • +AD5161: FAQ
  • +AD5203: FAQ
  • +AD5206: FAQ
  • +AD5222: FAQ
  • +AD5232: FAQ
  • +AD5235: FAQ
  • +AD5243: FAQ
  • +AD5245: FAQ
  • +AD5248: FAQ
  • +AD5251: FAQ
  • +AD5252: FAQ
  • +AD5254: FAQ
  • +AD5258: FAQ
  • +AD5259: FAQ
  • +AD5263: FAQ
  • +AD5270: FAQ
  • +AD5271: FAQ
  • +AD5272: FAQ
  • +AD5282: FAQ
  • +AD5290: FAQ
  • AD5292: FAQ
  • +AD5293: FAQ
  • +AD5593R: FAQ
  • +AD650: FAQ
  • +AD652: FAQ
  • +AD652SE: FAQ
  • +AD654: FAQ
  • +AD7142: FAQ
  • +AD7147: FAQ
  • +AD7148: FAQ
  • +AD7150: FAQ
  • +AD7151: FAQ
  • +AD7293: FAQ
  • +AD7400A: FAQ
  • +AD7401: FAQ
  • +AD7403: FAQ
  • +AD74115H: FAQ
  • +AD7415: FAQ
  • +AD7416: FAQ
  • +AD7417: FAQ
  • +AD7418: FAQ
  • +AD74416H - FAQ
  • +AD7740: FAQ
  • +AD7741: FAQ
  • +AD7745: FAQ
  • +AD7747: FAQ
  • +AD7879: FAQ
  • +AD8152: FAQ
  • +AD8156: FAQ
  • +AD8158: FAQ
  • +AD8159: FAQ
  • AD8400: FAQ
  • +AD8403: FAQ
  • +ADAQ4001: FAQ
  • +ADE7912: FAQ
  • +ADE7913: FAQ
  • +ADG3247: FAQ
  • +ADG3248: FAQ
  • +ADG3300: FAQ
  • +ADG3304: FAQ
  • +ADG3308: FAQ
  • +ADN4600: FAQ
  • +ADN4604: FAQ
  • +ADT7310: FAQ
  • +ADT7320: FAQ
  • +ADT7410: FAQ
  • +ADT7470: FAQ
  • +ADVFC32: FAQ
  • +DS1624: FAQ
  • +DS1629S+: FAQ
  • +DS1882: FAQ
  • +DS1882E-050+: FAQ
  • +DS3501U+: FAQ
  • +DS3502U+: FAQ
  • +DS3902U-515+: FAQ
  • +DS3930: FAQ
  • +DS75LVS+: FAQ
  • +HMC661: FAQ
  • +HMC953LC4B: FAQ
  • +MAX13003EEUE+: FAQ
  • +MAX13035EEBE+: FAQ
  • +MAX13035EETE+: FAQ
  • +MAX14001: FAQ
  • +MAX14001AAP+: FAQ
  • +MAX14591ETA+: FAQ
  • +MAX14595: FAQ
  • +MAX14611: FAQ
  • +MAX1617: FAQ
  • +MAX1617AMEE_T1: FAQ
  • +MAX1619: FAQ
  • +MAX1619MEE+: FAQ
  • +MAX1668MEE+: FAQ
  • +MAX2084CXL+: FAQ
  • +MAX22531: FAQ
  • +MAX3002: FAQ
  • +MAX3012EUP+: FAQ
  • +MAX3023EUD+: FAQ
  • +MAX31722MUA+: FAQ
  • +MAX31723MUA+: FAQ
  • +MAX31725MTA+T: FAQ
  • +MAX31730: FAQ
  • +MAX31855EASA+: FAQ
  • MAX31855KASA+: FAQ
  • +MAX31855KASA+T: FAQ
  • +MAX31855PMB1#: FAQ
  • +MAX31856: FAQ
  • +MAX31856EVSYS#: FAQ
  • MAX31856MUD+: FAQ
  • +MAX31856MUD+T: FAQ
  • +MAX31865 RTD-DIGIT: FAQ
  • +MAX31865: FAQ
  • -MAX31865AAP+: FAQ
    • Can MAX31865 SPI interface be used in daisy chain?
    • Can the MAX31865 operate with RTD sensors other than PT-100 to PT-1000, for example a Ni-120?
    • Capacitor Value for MAX31865
    • How should the FORCE2 pin of the MAX31865 be connected when operating in a 2 or 4 wire RTD configuration?
    • MAX31865 does not generate any output voltage at its bias pin even though it should be 2.0V under normal operation. From the typical application circuits, there should be valid Vbias with 3.3V power supply and GND properly connected. What might be the reas
    • What are the recommended values of C1 in the MAX31865 typical application circuit?
    • When using PT100, can I use a resistor with a value slightly different from 400 ohm (e.g 402 ohms) for external reference resistor of the MAX31865?
    • Why is RTD DATA REG not consistent with the ADC code value in table 9 of the datasheet of the MAX31865 (Rev 3 7/15)?
  • MAX31865ATP+: FAQ
  • +MAX31865ATP+T: FAQ
  • +MAX31865EVKIT#: FAQ
  • +MAX31875A/D+: FAQ
  • +MAX31875R1TZS+: FAQ
  • +MAX3373EEBL+: FAQ
  • +MAX3378EEUD+: FAQ
  • +MAX3390E: FAQ
  • +MAX3397EELA+: FAQ
  • +MAX5417LETA+: FAQ
  • +MAX5422: FAQ
  • +MAX5433LETA+: FAQ
  • +MAX5479ETE+: FAQ
  • +MAX5481: FAQ
  • +MAX5483ETE+: FAQ
  • +MAX5483EUD: FAQ
  • +MAX5484ETE+: FAQ
  • +MAX5484EUD+: FAQ
  • +MAX5487ETE+: FAQ
  • +MAX5494: FAQ
  • +MAX5860: FAQ
  • +MAX6575LZUT+: FAQ
  • +MAX6581_TG98+_A1: FAQ
  • +MAX6618AUB+: FAQ
  • +MAX6621: FAQ
  • +MAX6625PMUT-T: FAQ
  • +MAX6626PMUT#G16: FAQ
  • +MAX6627MKA#G16: FAQ
  • +MAX6630MUT: FAQ
  • +MAX6633MSA+: FAQ
  • +MAX6635EVKIT+: FAQ
  • +MAX6652AUB+: FAQ
  • +MAX6655: FAQ
  • +MAX6682MUA+: FAQ
  • +MAX6689: FAQ
  • +MAX6691MUB+: FAQ
  • +MAX6696AEE+T: FAQ
  • +MAX6698EE99+: FAQ
  • +MAX7500ASA/V+: FAQ
  • +MAX9110EKA+: FAQ
  • +MAX9112EKA+T: FAQ
  • +MAX9123ESE_T1: FAQ
  • +MAX9123EUE+: FAQ
  • +MAX9130EXT+: FAQ
  • MAX9205: FAQ
  • +MAX9206ETI+: FAQ
  • +MAX9217: FAQ
  • +MAX9257A: FAQ
  • +MAX9258AGCM/V+: FAQ
  • +MAX9310AEUP+: FAQ
  • +MAX9315: FAQ
  • +MAX9370ESA+: FAQ
  • +MAX9377EUA+: FAQ
  • +MAX9378: FAQ
  • MAX96715: FAQ
  • +MAX96715GTG/V+: FAQ
  • +MAX96717FGTJ/V+: FAQ
  • +MAX96717_TJ/VY+_A1: FAQ
  • +RDC1740: FAQ
  • +AD5292BRUZ-50: FAQ
  • +AD9834: FAQ

What are the recommended values of C1 in the MAX31865 typical application circuit?

Only two capacitor values are recommended in the datasheet for two values of  RTD resistor. Can we use other values of RTDs also?

The device is optimized for Platinum based RTDs. However, any RTD can be used. The constants of the Callendar-Van Dusen equation will be different for different RTDs

R(T) = R0(1 + AT + BT2 + C(T - 100)T3)

Where

T = temperature (degrees C)

R(T) = resistance at T

R0 = resistance at T = 0 degrees C

Where constants A, B, and C are derived from experimentally determined parameters α, β, and δ using resistance measurements for each made at 0°C, 100°C and 260°C.

These constants vary from RTD to RTD.

Again selection of capacitor depends on the resistance of the RTD used and your choice of cutoff frequency.

Tags: MAX31865AAP+ Digital Temperature Sensors Integrated/Special Purpose A/D Converters KA-03673 MAX31865