Question
How could I choose the closed-loop bandwidth (fBW with the AD2S80A
Are there guidelines.
Resolution Ratio of Reference Frequency/Bandwidth
10 2.5 : 1
12 4 : 1
14 6 : 1
16 7.5 : 1
Could you please help to give some comments on it? Thanks.
Answer
That section is a little confusing I agree.
The data sheet states,
5. Closed-Loop Bandwidth Selection (C4, C5, R5)
a. Choose the closed-loop bandwidth (fBW) required
ensuring that the ratio of reference frequency to bandwidth
does not exceed the following guidelines:
Resolution Ratio of Reference Frequency/Bandwidth
10 2.5 : 1
12 4 : 1
14 6 : 1
16 7.5 : 1
Typical values may be 100 Hz for a 400 Hz reference frequency
and 500 Hz to 1000 Hz for a 5 kHz reference frequency.
This would be better interpreted as choose a bandwidth at least the ratios
mentioned.
For example with 12 bits resolution and a 5 kHz reference frequency the
bandwidth should be 1.25kHz maximum but down to 500Hz or a 10:1 ratio should be
fine.
If the customer continues to have trouble determining the component values I
can provide some assistance or I suggest the component selection program. It
can be found at
http://ez.analog.com/message/41875#41875
if you scroll down through the text.