Question
What is the maximum acceptable clock rise time for reliable operation of the
AD5160?
Answer
When using the SPI Interface, it is assumed that the master has strong drivers
so that the input buffers don't have hysteresis. To summarize, we cannot
predict the buffers behaviour when the input signal is between Vil<Vin
Furthermore it depends on the temperature and the components deviation (skews).
So, you should guarantee sufficiently fast rising and falling edges and in
other words use external buffers.