Question
Can 2 AD2S80As be used with the same inductosyn?
Answer
Yes, but they must have the same reference frequency from the same excitation
source.
I don't see any problem in principle with connecting two AD2S80A components to
the same output. Both devices have an input buffer so they shouldn't load the
pre amp output. I assume that both outputs will receive the same reference
frequency from the excitation source.