Question
I'd like to be able to read the data the AD7746 Evaluation Board is producing
into my own software,
but I can't find any information on this?
Answer
The evaluation system contains our CDC component, which we want customers to
evaluate
and to which we are, of course, prepared to provide full support for.
The evaluation system also includes a third party (Cypress) USB microcontroller
in order to allow connection to PC via USB interface. We provide user interface
software for the PC to use the evaluation setup in order to perform data
acquisition and basic analysis.
We cannot support a connection of the Cypress uC via the USB interface to a
customer specific system, a system which is to us is unknown and unspecified.
We
have only limited knowledge of the Cypress controller and drivers ourselves,
the DLL that we use on PC are documented very little. We cannot provide support
for that third party component in our evaluation system.
However it is possible to make some Labview example code available. This
Labview example code uses all components required to access the CDC on the
evaluation board via Labview on the PC. The overall functionality can be
adapted by the customer.