Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Data Converters
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Data Converters
Data Converters
Documents Using MAX31855KASA, the result read(0x7D5023D0) indicates that there are no malfunctions. However, the thermocouple temperature is 2005 degree C, and the reference junction temperature is 35.81 degree C, which is incorrect.
  • Files
  • FAQs/Docs
  • Members
  • Sub-Groups
  • Tags
  • Cancel

Products Mentioned

MAX31855 Production
The MAX31855 performs cold-junction compensation and digitizes the signal from a K-, J-, N-, T-, S-, R-, or E-type thermocouple. The data is output in...
Datasheet
MAX31855 on Analog.com

Associated Drivers

Table of Contents
  • DATA CONVERTERS SUPPORT COMMUNITY
  • +Documents (More FAQs in Sub-Groups)
  • +AD7730: FAQ
  • +AD7746: FAQ
  • +ADC: FAQ
  • +AD1871: FAQ
  • +AD1877: FAQ
  • +AD1974: FAQ
  • +AD2S1200: FAQ
  • +AD2S1205: FAQ
  • +AD2S1210: FAQ
  • +AD2S80A: FAQ
  • +AD2S83: FAQ
  • +AD2S90: FAQ
  • +AD4080: FAQ
  • +AD4081: FAQ
  • +AD4083: FAQ
  • +AD4084: FAQ
  • +AD4086: FAQ
  • +AD4087: FAQ
  • +AD4880: FAQ
  • +AD4883: FAQ
  • +AD4884: FAQ
  • +AD5111: FAQ
  • +AD5112: FAQ
  • +AD5115: FAQ
  • +AD5116: FAQ
  • +AD5121: FAQ
  • +AD5141: FAQ
  • +AD5141BCPZ100-RL7: FAQ
  • +AD5142: FAQ
  • +AD5160: FAQ
  • +AD5161: FAQ
  • +AD5203: FAQ
  • +AD5206: FAQ
  • +AD5222: FAQ
  • +AD5232: FAQ
  • +AD5235: FAQ
  • +AD5243: FAQ
  • +AD5245: FAQ
  • +AD5248: FAQ
  • +AD5251: FAQ
  • +AD5252: FAQ
  • +AD5254: FAQ
  • +AD5258: FAQ
  • +AD5259: FAQ
  • +AD5263: FAQ
  • +AD5270: FAQ
  • +AD5271: FAQ
  • +AD5272: FAQ
  • +AD5282: FAQ
  • +AD5290: FAQ
  • AD5292: FAQ
  • +AD5293: FAQ
  • +AD5593R: FAQ
  • +AD650: FAQ
  • +AD652: FAQ
  • +AD652SE: FAQ
  • +AD654: FAQ
  • +AD7142: FAQ
  • +AD7147: FAQ
  • +AD7148: FAQ
  • +AD7150: FAQ
  • +AD7151: FAQ
  • +AD7293: FAQ
  • +AD7400A: FAQ
  • +AD7401: FAQ
  • +AD7403: FAQ
  • +AD74115H: FAQ
  • +AD7415: FAQ
  • +AD7416: FAQ
  • +AD7417: FAQ
  • +AD7418: FAQ
  • +AD74416H - FAQ
  • +AD7740: FAQ
  • +AD7741: FAQ
  • +AD7745: FAQ
  • +AD7747: FAQ
  • +AD7879: FAQ
  • +AD8152: FAQ
  • +AD8156: FAQ
  • +AD8158: FAQ
  • +AD8159: FAQ
  • AD8400: FAQ
  • +AD8403: FAQ
  • +ADAQ4001: FAQ
  • +ADE7912: FAQ
  • +ADE7913: FAQ
  • +ADG3247: FAQ
  • +ADG3248: FAQ
  • +ADG3300: FAQ
  • +ADG3304: FAQ
  • +ADG3308: FAQ
  • +ADN4600: FAQ
  • +ADN4604: FAQ
  • +ADT7310: FAQ
  • +ADT7320: FAQ
  • +ADT7410: FAQ
  • +ADT7470: FAQ
  • +ADVFC32: FAQ
  • +DS1624: FAQ
  • +DS1629S+: FAQ
  • +DS1882: FAQ
  • +DS1882E-050+: FAQ
  • +DS3501U+: FAQ
  • +DS3502U+: FAQ
  • +DS3902U-515+: FAQ
  • +DS3930: FAQ
  • +DS75LVS+: FAQ
  • +HMC661: FAQ
  • +HMC953LC4B: FAQ
  • +MAX13003EEUE+: FAQ
  • +MAX13035EEBE+: FAQ
  • +MAX13035EETE+: FAQ
  • +MAX14001: FAQ
  • +MAX14001AAP+: FAQ
  • +MAX14591ETA+: FAQ
  • +MAX14595: FAQ
  • +MAX14611: FAQ
  • +MAX1617: FAQ
  • +MAX1617AMEE_T1: FAQ
  • +MAX1619: FAQ
  • +MAX1619MEE+: FAQ
  • +MAX1668MEE+: FAQ
  • +MAX2084CXL+: FAQ
  • +MAX22531: FAQ
  • +MAX3002: FAQ
  • +MAX3012EUP+: FAQ
  • +MAX3023EUD+: FAQ
  • +MAX31722MUA+: FAQ
  • +MAX31723MUA+: FAQ
  • +MAX31725MTA+T: FAQ
  • +MAX31730: FAQ
  • +MAX31855EASA+: FAQ
  • MAX31855KASA+: FAQ
  • -MAX31855KASA+T: FAQ
    • Can I drive the MAX31855 SPI pins with a 5V supply?
    • Can the MAX31855EVKIT work with an E-type thermocouple?
    • Does the MAX31855 have any filtering for EMI or RF frequencies?
    • Does the MAX31855 linearize the thermocouple result?
    • I am experiencing temperature errors due to noise induced on the thermocouple cable. Can I connect the T- terminal to the GND of the MAX31855 to help eliminate that error?
    • Is the SDO (data out) pin of MAX31855 tri-stated ?
    • MAX31855TASA 测量负温度问题误差很大,如何解决?
    • To realize multi-channel thermocouple temperature measurement with multiple MAX31855 chips, can the T- of multiple MAX31855's be connected together?
    • Using MAX31855KASA, the result read(0x7D5023D0) indicates that there are no malfunctions. However, the thermocouple temperature is 2005 degree C, and the reference junction temperature is 35.81 degree C, which is incorrect.
    • What could cause large errors between a generated signal and measured values for a thermocouple when interfacing to the MAX31855K?
    • What is the temperature conversion behavior of the MAX31855 if the thermocouple leads are connected in reverse?
    • Which SPI mode does the MAX31855 use?
  • +MAX31855PMB1#: FAQ
  • +MAX31856: FAQ
  • +MAX31856EVSYS#: FAQ
  • MAX31856MUD+: FAQ
  • +MAX31856MUD+T: FAQ
  • +MAX31865 RTD-DIGIT: FAQ
  • +MAX31865: FAQ
  • +MAX31865AAP+: FAQ
  • MAX31865ATP+: FAQ
  • +MAX31865ATP+T: FAQ
  • +MAX31865EVKIT#: FAQ
  • +MAX31875A/D+: FAQ
  • +MAX31875R1TZS+: FAQ
  • +MAX3373EEBL+: FAQ
  • +MAX3378EEUD+: FAQ
  • +MAX3390E: FAQ
  • +MAX3397EELA+: FAQ
  • +MAX5417LETA+: FAQ
  • +MAX5422: FAQ
  • +MAX5433LETA+: FAQ
  • +MAX5479ETE+: FAQ
  • +MAX5481: FAQ
  • +MAX5483ETE+: FAQ
  • +MAX5483EUD: FAQ
  • +MAX5484ETE+: FAQ
  • +MAX5484EUD+: FAQ
  • +MAX5487ETE+: FAQ
  • +MAX5494: FAQ
  • +MAX5860: FAQ
  • +MAX6575LZUT+: FAQ
  • +MAX6581_TG98+_A1: FAQ
  • +MAX6618AUB+: FAQ
  • +MAX6621: FAQ
  • +MAX6625PMUT-T: FAQ
  • +MAX6626PMUT#G16: FAQ
  • +MAX6627MKA#G16: FAQ
  • +MAX6630MUT: FAQ
  • +MAX6633MSA+: FAQ
  • +MAX6635EVKIT+: FAQ
  • +MAX6652AUB+: FAQ
  • +MAX6655: FAQ
  • +MAX6682MUA+: FAQ
  • +MAX6689: FAQ
  • +MAX6691MUB+: FAQ
  • +MAX6696AEE+T: FAQ
  • +MAX6698EE99+: FAQ
  • +MAX7500ASA/V+: FAQ
  • +MAX9110EKA+: FAQ
  • +MAX9112EKA+T: FAQ
  • +MAX9123ESE_T1: FAQ
  • +MAX9123EUE+: FAQ
  • +MAX9130EXT+: FAQ
  • MAX9205: FAQ
  • +MAX9206ETI+: FAQ
  • +MAX9217: FAQ
  • +MAX9257A: FAQ
  • +MAX9258AGCM/V+: FAQ
  • +MAX9310AEUP+: FAQ
  • +MAX9315: FAQ
  • +MAX9370ESA+: FAQ
  • +MAX9377EUA+: FAQ
  • +MAX9378: FAQ
  • MAX96715: FAQ
  • +MAX96715GTG/V+: FAQ
  • +MAX96717FGTJ/V+: FAQ
  • +MAX96717_TJ/VY+_A1: FAQ
  • +RDC1740: FAQ
  • +AD5292BRUZ-50: FAQ
  • +AD9834: FAQ

Using MAX31855KASA, the result read(0x7D5023D0) indicates that there are no malfunctions. However, the thermocouple temperature is 2005 degree C, and the reference junction temperature is 35.81 degree C, which is incorrect.


There are two possible causes of this problem:

1. SPI communication error. If the reference junction temperature is confirmed to be at 35 degree, the reference junction reading is correct. If the temperature at the reference junction is not at 35 degree, this result is incorrect. We can try to increase the temperature around MAX31855 and see if the temperature read at the reference junction is correct.

2. The time interval between two readings is too short. The conversion time of MAX31855 is 100ms. Therefore, after reading the temperature conversion result, we must wait for at least 100ms before starting the next reading. After the reading is complete, CS must be pulled up. Upon power up, CS should be pulled up, and the temperature can be read 200ms later.
Tags: MAX31855KASA+ Digital Temperature Sensors 000101316 MAX31855 Integrated/Special Purpose A/D Converters