Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      World Engineering Day Quiz!

      By Kuo-Chang A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

EngineerZone
EngineerZone
Data Converters
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Data Converters
Data Converters
Documents Is the first 14 bit data read out already cold-junction compensated for MAX31855?
  • Files
  • FAQs/Docs
  • Members
  • Sub-Groups
  • Tags
  • Cancel

Products Mentioned

MAX31855 Production
The MAX31855 performs cold-junction compensation and digitizes the signal from a K-, J-, N-, T-, S-, R-, or E-type thermocouple. The data is output in...
Datasheet
MAX31855 on Analog.com

Table of Contents
  • DATA CONVERTERS SUPPORT COMMUNITY
  • +Documents (More FAQs in Sub-Groups)
  • +AD7730: FAQ
  • +AD7746: FAQ
  • +ADC: FAQ
  • +AD1871: FAQ
  • +AD1877: FAQ
  • +AD1974: FAQ
  • +AD2S1200: FAQ
  • +AD2S1205: FAQ
  • +AD2S1210: FAQ
  • +AD2S80A: FAQ
  • +AD2S83: FAQ
  • +AD2S90: FAQ
  • +AD4080: FAQ
  • +AD4081: FAQ
  • +AD4083: FAQ
  • +AD4084: FAQ
  • +AD4086: FAQ
  • +AD4087: FAQ
  • +AD4880: FAQ
  • +AD4883: FAQ
  • +AD4884: FAQ
  • +AD5111: FAQ
  • +AD5112: FAQ
  • +AD5115: FAQ
  • +AD5116: FAQ
  • +AD5121: FAQ
  • +AD5141: FAQ
  • +AD5141BCPZ100-RL7: FAQ
  • +AD5142: FAQ
  • +AD5160: FAQ
  • +AD5161: FAQ
  • +AD5203: FAQ
  • +AD5206: FAQ
  • +AD5222: FAQ
  • +AD5232: FAQ
  • +AD5235: FAQ
  • +AD5243: FAQ
  • +AD5245: FAQ
  • +AD5248: FAQ
  • +AD5251: FAQ
  • +AD5252: FAQ
  • +AD5254: FAQ
  • +AD5258: FAQ
  • +AD5259: FAQ
  • +AD5263: FAQ
  • +AD5270: FAQ
  • +AD5271: FAQ
  • +AD5272: FAQ
  • +AD5282: FAQ
  • +AD5290: FAQ
  • AD5292: FAQ
  • +AD5293: FAQ
  • +AD5593R: FAQ
  • +AD650: FAQ
  • +AD652: FAQ
  • +AD652SE: FAQ
  • +AD654: FAQ
  • +AD7142: FAQ
  • +AD7147: FAQ
  • +AD7148: FAQ
  • +AD7150: FAQ
  • +AD7151: FAQ
  • +AD7293: FAQ
  • +AD7400A: FAQ
  • +AD7401: FAQ
  • +AD7403: FAQ
  • +AD74115H: FAQ
  • +AD7415: FAQ
  • +AD7416: FAQ
  • +AD7417: FAQ
  • +AD7418: FAQ
  • +AD74416H - FAQ
  • +AD7740: FAQ
  • +AD7741: FAQ
  • +AD7745: FAQ
  • +AD7747: FAQ
  • +AD7879: FAQ
  • +AD8152: FAQ
  • +AD8156: FAQ
  • +AD8158: FAQ
  • +AD8159: FAQ
  • AD8400: FAQ
  • +AD8403: FAQ
  • +ADAQ4001: FAQ
  • +ADE7912: FAQ
  • +ADE7913: FAQ
  • +ADG3247: FAQ
  • +ADG3248: FAQ
  • +ADG3300: FAQ
  • +ADG3304: FAQ
  • +ADG3308: FAQ
  • +ADN4600: FAQ
  • +ADN4604: FAQ
  • +ADT7310: FAQ
  • +ADT7320: FAQ
  • +ADT7410: FAQ
  • +ADT7470: FAQ
  • +ADVFC32: FAQ
  • +DS1624: FAQ
  • +DS1629S+: FAQ
  • +DS1882: FAQ
  • +DS1882E-050+: FAQ
  • +DS3501U+: FAQ
  • +DS3502U+: FAQ
  • +DS3902U-515+: FAQ
  • +DS3930: FAQ
  • +DS75LVS+: FAQ
  • +HMC661: FAQ
  • +HMC953LC4B: FAQ
  • +MAX13003EEUE+: FAQ
  • +MAX13035EEBE+: FAQ
  • +MAX13035EETE+: FAQ
  • +MAX14001: FAQ
  • +MAX14001AAP+: FAQ
  • +MAX14591ETA+: FAQ
  • +MAX14595: FAQ
  • +MAX14611: FAQ
  • +MAX1617: FAQ
  • +MAX1617AMEE_T1: FAQ
  • +MAX1619: FAQ
  • +MAX1619MEE+: FAQ
  • +MAX1668MEE+: FAQ
  • +MAX2084CXL+: FAQ
  • +MAX22531: FAQ
  • +MAX3002: FAQ
  • +MAX3012EUP+: FAQ
  • +MAX3023EUD+: FAQ
  • +MAX31722MUA+: FAQ
  • +MAX31723MUA+: FAQ
  • +MAX31725MTA+T: FAQ
  • +MAX31730: FAQ
  • -MAX31855EASA+: FAQ
    • Can the MAX31855 support ungrounded, grounded, and exposed thermocouples?
    • Does any MAX31855 version support all thermocouple types?
    • Does MAX31855 support B-type thermocouples?
    • For the MAX31855, does the thermocouple temperature data require linearization?
    • How many MAX31855 ICs can be connected to a single SPI master?
    • I am getting some error in the thermocouple result of the MAX31855. What could be the cause of that?
    • If there is noise on the voltage supply to the MAX31855, should a low noise voltage regulator be implemented to reduce the temperature conversion error?
    • In the MAX31855, how is the reference junction temperature data used?
    • Is it possible to achieve a higher sampling rate from the MAX31855
    • Is the first 14 bit data read out already cold-junction compensated for MAX31855?
    • Is the SO output of the MAX31855 an open collector (open-drain) or push-pull structure?
    • Multiplexing multiple thermocouples using MAX31855?
    • The MAX31855EVKIT uses Omega connectors, can I use an alternative connector?
    • Using the MAX31855 and external switches to achieve multi-channel temperature conversion, I noticed that some delay needs to be added after switching channel to avoid interference. How do I solve the problem?
    • What are the main differences between the MAX31855 and the MAX31856?
    • What happens if /CS is driven high during data transmission?
    • What happens if I increase the differential capacitance between the T+ and T- pins on the MAX31855?
    • What is Maxim's best alternative to obsolete part MAX6675?
    • What is the purpose of the 12-bit Internal Temperature in MAX31855?
    • When does MAX31855's temperature conversion begin, and how are the different conversion stages triggered?
  • MAX31855KASA+: FAQ
  • +MAX31855KASA+T: FAQ
  • +MAX31855PMB1#: FAQ
  • +MAX31856: FAQ
  • +MAX31856EVSYS#: FAQ
  • MAX31856MUD+: FAQ
  • +MAX31856MUD+T: FAQ
  • +MAX31865 RTD-DIGIT: FAQ
  • +MAX31865: FAQ
  • +MAX31865AAP+: FAQ
  • MAX31865ATP+: FAQ
  • +MAX31865ATP+T: FAQ
  • +MAX31865EVKIT#: FAQ
  • +MAX31875A/D+: FAQ
  • +MAX31875R1TZS+: FAQ
  • +MAX3373EEBL+: FAQ
  • +MAX3378EEUD+: FAQ
  • +MAX3390E: FAQ
  • +MAX3397EELA+: FAQ
  • +MAX5417LETA+: FAQ
  • +MAX5422: FAQ
  • +MAX5433LETA+: FAQ
  • +MAX5479ETE+: FAQ
  • +MAX5481: FAQ
  • +MAX5483ETE+: FAQ
  • +MAX5483EUD: FAQ
  • +MAX5484ETE+: FAQ
  • +MAX5484EUD+: FAQ
  • +MAX5487ETE+: FAQ
  • +MAX5494: FAQ
  • +MAX5860: FAQ
  • +MAX6575LZUT+: FAQ
  • +MAX6581_TG98+_A1: FAQ
  • +MAX6618AUB+: FAQ
  • +MAX6621: FAQ
  • +MAX6625PMUT-T: FAQ
  • +MAX6626PMUT#G16: FAQ
  • +MAX6627MKA#G16: FAQ
  • +MAX6630MUT: FAQ
  • +MAX6633MSA+: FAQ
  • +MAX6635EVKIT+: FAQ
  • +MAX6652AUB+: FAQ
  • +MAX6655: FAQ
  • +MAX6682MUA+: FAQ
  • +MAX6689: FAQ
  • +MAX6691MUB+: FAQ
  • +MAX6696AEE+T: FAQ
  • +MAX6698EE99+: FAQ
  • +MAX7500ASA/V+: FAQ
  • +MAX9110EKA+: FAQ
  • +MAX9112EKA+T: FAQ
  • +MAX9123ESE_T1: FAQ
  • +MAX9123EUE+: FAQ
  • +MAX9130EXT+: FAQ
  • MAX9205: FAQ
  • +MAX9206ETI+: FAQ
  • +MAX9217: FAQ
  • +MAX9257A: FAQ
  • +MAX9258AGCM/V+: FAQ
  • +MAX9310AEUP+: FAQ
  • +MAX9315: FAQ
  • +MAX9370ESA+: FAQ
  • +MAX9377EUA+: FAQ
  • +MAX9378: FAQ
  • MAX96715: FAQ
  • +MAX96715GTG/V+: FAQ
  • +MAX96717FGTJ/V+: FAQ
  • +MAX96717_TJ/VY+_A1: FAQ
  • +RDC1740: FAQ
  • +AD5292BRUZ-50: FAQ
  • +AD9834: FAQ

Is the first 14 bit data read out already cold-junction compensated for MAX31855?

Yes, the data read out as the first 14 bits compensates for cold-junction using the linear correction formula. Allow 200ms after start-up before reading data, you may read every 100ms thereafter. See "Temperature Conversion" section on page 8 of the datasheet for more details.
Tags: Digital Temperature Sensors 000095989 MAX31855 Integrated/Special Purpose A/D Converters MAX31855EASA+