Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC's Quiz AQQ298 about an interlaced square and triangle puzzle

      1. Quote of the month: " Behind every great man is a woman rolling her eyes " - Jim Carrey 2. New quiz AQQ298 about an interlaced square and triangle...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

EngineerZone
EngineerZone
Data Converters
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Data Converters
Data Converters
Documents How do I interpret the full scale error of the MAX31856?
  • Files
  • FAQs/Docs
  • Members
  • Sub-Groups
  • Tags
  • Cancel
  • DATA CONVERTERS SUPPORT COMMUNITY
  • +Documents (More FAQs in Sub-Groups)
  • +AD7730: FAQ
  • +AD7746: FAQ
  • +ADC: FAQ
  • +AD1871: FAQ
  • +AD1877: FAQ
  • +AD1974: FAQ
  • +AD2S1200: FAQ
  • +AD2S1205: FAQ
  • +AD2S1210: FAQ
  • +AD2S80A: FAQ
  • +AD2S83: FAQ
  • +AD2S90: FAQ
  • +AD4080: FAQ
  • +AD4081: FAQ
  • +AD4083: FAQ
  • +AD4084: FAQ
  • +AD4086: FAQ
  • +AD4087: FAQ
  • +AD4880: FAQ
  • +AD4883: FAQ
  • +AD4884: FAQ
  • +AD5111: FAQ
  • +AD5112: FAQ
  • +AD5115: FAQ
  • +AD5116: FAQ
  • +AD5121: FAQ
  • +AD5141: FAQ
  • +AD5141BCPZ100-RL7: FAQ
  • +AD5142: FAQ
  • +AD5160: FAQ
  • +AD5161: FAQ
  • +AD5203: FAQ
  • +AD5206: FAQ
  • +AD5222: FAQ
  • +AD5232: FAQ
  • +AD5235: FAQ
  • +AD5243: FAQ
  • +AD5245: FAQ
  • +AD5248: FAQ
  • +AD5251: FAQ
  • +AD5252: FAQ
  • +AD5254: FAQ
  • +AD5258: FAQ
  • +AD5259: FAQ
  • +AD5263: FAQ
  • +AD5270: FAQ
  • +AD5271: FAQ
  • +AD5272: FAQ
  • +AD5282: FAQ
  • +AD5290: FAQ
  • AD5292: FAQ
  • +AD5293: FAQ
  • +AD5593R: FAQ
  • +AD650: FAQ
  • +AD652: FAQ
  • +AD652SE: FAQ
  • +AD654: FAQ
  • +AD7142: FAQ
  • +AD7147: FAQ
  • +AD7148: FAQ
  • +AD7150: FAQ
  • +AD7151: FAQ
  • +AD7293: FAQ
  • +AD7400A: FAQ
  • +AD7401: FAQ
  • +AD7403: FAQ
  • +AD74115H: FAQ
  • +AD7415: FAQ
  • +AD7416: FAQ
  • +AD7417: FAQ
  • +AD7418: FAQ
  • +AD74416H - FAQ
  • +AD7740: FAQ
  • +AD7741: FAQ
  • +AD7745: FAQ
  • +AD7747: FAQ
  • +AD7879: FAQ
  • +AD8152: FAQ
  • +AD8156: FAQ
  • +AD8158: FAQ
  • +AD8159: FAQ
  • AD8400: FAQ
  • +AD8403: FAQ
  • +ADAQ4001: FAQ
  • +ADE7912: FAQ
  • +ADE7913: FAQ
  • +ADG3247: FAQ
  • +ADG3248: FAQ
  • +ADG3300: FAQ
  • +ADG3304: FAQ
  • +ADG3308: FAQ
  • +ADN4600: FAQ
  • +ADN4604: FAQ
  • +ADT7310: FAQ
  • +ADT7320: FAQ
  • +ADT7410: FAQ
  • +ADT7470: FAQ
  • +ADVFC32: FAQ
  • +DS1624: FAQ
  • +DS1629S+: FAQ
  • +DS1882: FAQ
  • +DS1882E-050+: FAQ
  • +DS3501U+: FAQ
  • +DS3502U+: FAQ
  • +DS3902U-515+: FAQ
  • +DS3930: FAQ
  • +DS75LVS+: FAQ
  • +HMC661: FAQ
  • +HMC953LC4B: FAQ
  • +MAX13003EEUE+: FAQ
  • +MAX13035EEBE+: FAQ
  • +MAX13035EETE+: FAQ
  • +MAX14001: FAQ
  • +MAX14001AAP+: FAQ
  • +MAX14591ETA+: FAQ
  • +MAX14595: FAQ
  • +MAX14611: FAQ
  • +MAX1617: FAQ
  • +MAX1617AMEE_T1: FAQ
  • +MAX1619: FAQ
  • +MAX1619MEE+: FAQ
  • +MAX1668MEE+: FAQ
  • +MAX2084CXL+: FAQ
  • +MAX22531: FAQ
  • +MAX3002: FAQ
  • +MAX3012EUP+: FAQ
  • +MAX3023EUD+: FAQ
  • +MAX31722MUA+: FAQ
  • +MAX31723MUA+: FAQ
  • +MAX31725MTA+T: FAQ
  • +MAX31730: FAQ
  • +MAX31855EASA+: FAQ
  • MAX31855KASA+: FAQ
  • +MAX31855KASA+T: FAQ
  • +MAX31855PMB1#: FAQ
  • +MAX31856: FAQ
  • +MAX31856EVSYS#: FAQ
  • MAX31856MUD+: FAQ
  • -MAX31856MUD+T: FAQ
    • Can I connect BIAS to TC+ instead of TC- on MAX31856, will this affect accuracy?
    • Can I interface InfraRed Thermocouple to MAX31856?
    • Does the /CS pin on the MAX31856 have an internal pull up? Can it be left floating?
    • Does the MAX31856 use a sample and hold at the input?
    • How do I interpret the full scale error of the MAX31856?
    • How to deal with 50Hz noise for Thermocouple?
    • In the MAX31856, if a series resistance is used to reduce noise from the thermocouple (as in Figure 8 of datasheet), can the BIAS output be connected directly to T-?
    • MAX31856 have voltage mode and code formula mentioned on datasheet P20.Could you please explain code formula theory?What is 1.6 and 2^17 mean of this formula?
    • MAX31856 Open Circuit Fault Detection not detected upon startup with no thermocouple attached
    • There is a OVUV Fault flagged in the MAX31856. Could Open Circuit Detection be engaged to pull the circuit out of the Fault state?
    • To lower system operation current, the MAX31856 is designated as single conversion during the design phase (ON Duty 1/60). However, for most components the standby currents are between 10uA -- 500uA. The data sheet mentions that the standby current is 5.25
    • Using the MAX31856 and have a OVUV Fault which is still there even when the fault is removed. What is the issue?
    • What could be causing erroneous faults conditions and random temperature shifts in the MAX31856?
    • What is causing the MAX31856 to experience large voltages/oscillations?
    • What is the purpose of the MAX31856EVKIT 150 ohm series resistors on the digital lines?
  • +MAX31865 RTD-DIGIT: FAQ
  • +MAX31865: FAQ
  • +MAX31865AAP+: FAQ
  • MAX31865ATP+: FAQ
  • +MAX31865ATP+T: FAQ
  • +MAX31865EVKIT#: FAQ
  • +MAX31875A/D+: FAQ
  • +MAX31875R1TZS+: FAQ
  • +MAX3373EEBL+: FAQ
  • +MAX3378EEUD+: FAQ
  • +MAX3390E: FAQ
  • +MAX3397EELA+: FAQ
  • +MAX5417LETA+: FAQ
  • +MAX5422: FAQ
  • +MAX5433LETA+: FAQ
  • +MAX5479ETE+: FAQ
  • +MAX5481: FAQ
  • +MAX5483ETE+: FAQ
  • +MAX5483EUD: FAQ
  • +MAX5484ETE+: FAQ
  • +MAX5484EUD+: FAQ
  • +MAX5487ETE+: FAQ
  • +MAX5494: FAQ
  • +MAX5860: FAQ
  • +MAX6575LZUT+: FAQ
  • +MAX6581_TG98+_A1: FAQ
  • +MAX6618AUB+: FAQ
  • +MAX6621: FAQ
  • +MAX6625PMUT-T: FAQ
  • +MAX6626PMUT#G16: FAQ
  • +MAX6627MKA#G16: FAQ
  • +MAX6630MUT: FAQ
  • +MAX6633MSA+: FAQ
  • +MAX6635EVKIT+: FAQ
  • +MAX6652AUB+: FAQ
  • +MAX6655: FAQ
  • +MAX6682MUA+: FAQ
  • +MAX6689: FAQ
  • +MAX6691MUB+: FAQ
  • +MAX6696AEE+T: FAQ
  • +MAX6698EE99+: FAQ
  • +MAX7500ASA/V+: FAQ
  • +MAX9110EKA+: FAQ
  • +MAX9112EKA+T: FAQ
  • +MAX9123ESE_T1: FAQ
  • +MAX9123EUE+: FAQ
  • +MAX9130EXT+: FAQ
  • MAX9205: FAQ
  • +MAX9206ETI+: FAQ
  • +MAX9217: FAQ
  • +MAX9257A: FAQ
  • +MAX9258AGCM/V+: FAQ
  • +MAX9310AEUP+: FAQ
  • +MAX9315: FAQ
  • +MAX9370ESA+: FAQ
  • +MAX9377EUA+: FAQ
  • +MAX9378: FAQ
  • MAX96715: FAQ
  • +MAX96715GTG/V+: FAQ
  • +MAX96717FGTJ/V+: FAQ
  • +MAX96717_TJ/VY+_A1: FAQ
  • +RDC1740: FAQ
  • +AD5292BRUZ-50: FAQ
  • +AD9834: FAQ

How do I interpret the full scale error of the MAX31856?

Revision Creation Date Revision Author
Current Revision 11 Feb 2026 4:17 AM EngineerZone
Revision #10 10 Feb 2026 1:50 PM MSDAPI
Revision #9 10 Feb 2026 1:50 PM MSDAPI
Revision #8 19 Dec 2023 1:44 PM MSDAPI
Revision #7 19 Dec 2023 9:49 AM MSDAPI
Revision #6 6 Dec 2023 11:55 AM MSDAPI
Revision #5 6 Dec 2023 11:44 AM MSDAPI
Revision #4 6 Dec 2023 10:12 AM MSDAPI
Revision #3 6 Dec 2023 9:51 AM MSDAPI
Revision #2 6 Dec 2023 9:47 AM MSDAPI
Revision #1 20 Jun 2018 2:57 AM MSDAPI
  • Compare Versions View current version