Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

FAQ: Selecting A Reference for the AD536x and AD537x DACs

Q.

How do I select a reference for the AD536x and AD537x DACs?

-----------------------------------------------------------------------------------

A.

A reference value from +2V to +5V can be used with the AD536x and AD537x. Using the default register values the output span will be four times the reference value, e.g. +12V when using a +3V reference.

 

The AD536x is factory calibrated using a 5V reference and has a default output range of -10V to +10V.

The AD537x is factory calibrated using a 3V reference and has a default output range of -4V to +8V.

General Information:

This document covers  the denseDAC family. AD536x  refers to the AD5360, AD5361, AD5362 and AD5363 eight and 16 channel DACs. AD537x refers to the AD5370, AD5371, AD5372 and AD5373 thirty two and 40 channel DACs.

Comments
Anonymous
Related