Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

FAQ: Selecting An Output Range for the AD536x and AD537x DACs

Q.

How do I select an output range for the AD536x and AD537x DACs?

----------------------------------------------------------------

A.

The output span of the AD536x and AD537x is principally determined by the reference voltage on the VREFx pins. The m registers can be used to compact the range if required. See FAQ: Using the m and c Registers on AD536x and AD537x DACs for more information.

 

The output range can be controlled by programming the Offset register The offset register controls a 14-bit DAC. The AD5371 has 3 offset DACs while the other parts have 2 offset DACs. The offset DAC can be programmed to move the output span up or down. For example, the AD537x has a default range of -4V to +8V. By programming the Offset DACs this can be changed to -5V to +7V or -3V to +9V. The output range is subject to headroom and footroom limitations.

General Information:

This document covers the denseDAC family. AD536x refers to the AD5360, AD5361, AD5362 and AD5363 eight and 16 channel DACs. AD537x refers to the AD5370, AD5371, AD5372 and AD5373 thirty two and 40 channel DACs.

Comments
Anonymous
Related