Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question.
What is the value of thermal resistance theta JC(Junction-to-Case). Theta JA(Junction-to-Ambient) is shown at the data sheet. But theta JC is not there.
For the 64 LFCSP 9x9x0.85mm package, I see a number of ~0.2°C/W for Psi Jt. This is a calculated/simulated number based on a JEDEC 4 layer test board. JC is Junction to Case, JA is Junction to Air. We've specified Theta JA on the datasheet with a value of 20degree/W. Again this is specified for the package with the paddle soldered as recommended. Theta JC would be lower than this. Psi-Jt is a calculation of the silicon to package case differential when mounted on a PCB. This is a more accurate method than Theta-Jc for the customer to determine the temperature of the silicon (by measuring the package surface), as Theta-Jc is measured using infinite heat sinks and no PCB.