Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

AD5065 t7 maximum timing

I'd like to have information about the maximum required timing on t7 on the
AD5065 datasheet. I don't understand why the SYNC signal should be brought to
high in less than 30ns. I don't understand why, and chiefly I'm not able to
manage this from my FPGA, running with a 20MHz clock (50ns step for the
management of my SPI -> 10 MHz SPI clock). This requirement is really
surprising, and I guess this would not be respected by most of the
microcontroller's integrated SPI peripherals.
So I need your help to make me understand if this timing is really required in
any case, or if it is required to cover, for instance, the protocol with a
50MHz SPI Clock, or in some particular case. Moreover, my SPI clock is not
activated during SYNC=1 so perhaps this
requirement is not applicable in this case ?

 

The t7 parameter max of 30ns is due to a digital bug. There is a workaround
where you can use a software LDAC to update the output. If you keep /LDAC high
and use command 0010 or 0011 (table 8) to update the DACs you don't need to
adhere to the 30ns spec.

Comments
Anonymous
Related