Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

AD5290: Nominal resistance

You state the Nominal resistance tolerance as being +/- 30% in Rheostat mode,
what is the typical production spared in tolerance?

I realize the 'stock' answer would be +/- 30%, but this I feel, is the absolute
minimum and maximum to cover all eventualities.

 

+/-30% is the maximum part-to-part tolerance that we specify, and is a
measurement at 25degC. The temperature coefficient is in addition to the +/-30%
inital part-to-part spread.

Each lot is likely to have a spread that is less than +/-30%, and any outlying
parts are scrapped in final test (at ADIs expense.)

To give you an idea of the historic spread in total resistance (R_AB), devices
which passed have generally been well within the test limits, and only a few
devices were totally outside the max/min test limits (reject devices)
To take the 50k device as an example, the mean has been about 53k although it
has been up as high as 55k and down as low as 52k.
The (mean + 3sigma) distribution has been over 61k for some lots and the (mean
- 3sigma) has been down as far as 47k for some lots, although lately the (mean
+3 sigma) has been around 57k and the (mean - 3sigma) around 50.5k.

Having said all this, it is quite possible for us to ship a batch of devices in
the future whose resistance is at the upper or lower extreme of the
specification, and you would have no right to a refund or an explanation, or to
request devices from a different batch that happens to work in your
application.

In order to design to a tighter tolerance you would need a means of screening
devices before they are populated on the board (to avoid expensive board
rework).

You would also need to accept the responsibility for scrapping any devices that
don't meet your tighter specifications. As well as the financial cost, there
can also be operational implications if you can't get hold of devices which
meet your tighter limits for an extended period, because our process has
shifted for whatever reason.

So my advice would be to use the +/-30% specification if you are using the
device in Rheostat mode. If you need a tighter tolerance, you might consider
using a circuit which depends on the matching between Raw and Rwb in the same
IC or the matching between Rab on a DUAL potentiometer IC. e.g. the AD5262 are
dual pots with channel resistance matching of typically 0.1%.

Comments
Anonymous
Parents Comment Children
Related