Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

AD5293: shift register DIN with MSB first or least?

Which bit must be sent first from the microcontroller to DIN - bit 15 or bit 0?
The Datasheet contains two conflicting descriptions: In the timing diagram on
page 8, D0 = LSB first sent from the microcontroller. From page 18 'Shift
Register', I understand that bit 15 = MSB is sent first by the microcontroller.
Which description is correct?

 

The MSB should be shifted first. Figure 4 is probably a bit confusing but when
the data is sampled (falling edge of \SYNC) the data is X.

Comments
Anonymous
Related