Q
Hello, by testing more or less 10 AD5338s I find an offset from 3mV to 17mV
only for 2nd channel VoutB (PIN3)
while VoutA (PIN2) has no offset. I tested the pin with no load. The amount of
offset is in the tolerance (from datasheet) but I don't understand why it is
present only on the 2nd channel.
Do you know some issue regarding a lower offset-performance for 2nd channel or
some external causes that can influence
the offset-perfomance?
A
There is a different layout for different channels so the offset and gain can
be different. Each channel will not have the same offset and would need to
calibrated separately.