Search FAQs on the left to see if your question has been answered. Click on the dropdown to view all of the documents associated with the product. If you can't find your question, click on Ask a Question

Error in Figure 32 - 2-wire serial bus

In the Serial Interface section on page 19 in the datasheet it says:

“The 2-wire serial bus protocol operates as follows: the master initiates data
transfer by establishing a start condition when a high-to-low transition on the
SDA line occurs while SCL is high.”

However, in Figure 32 on the same page it looks like the write starts after a
high-to-low transition on the SDA line while SCL is low.

Is there an error in Figure 32? Can you clarify what is the correct way to
start a data transmission?

 

The start condition for 2-wire serial bus protocol is when a high-to-low
transition on the SDA line occurs while SCL is high, as shown in Figure 2, page
6, in the www.analog.com/AD5593R datasheet.

In Figure 32 on page 19 of the datasheet there is an error. In fact, the
falling edge of the SDA should happen a bit more to the left, where SCL is
high. This will be corrected at the next revision of the datasheet.

Comments
Anonymous
Related