Question
I would like to calculate the total temp. Coefficient of this component.
If i use the RFB as the feedback resistor of the external Amp. and connect an
external Ref. what is the total temp. Coefficient with respect to the following
Spec's:
1. Gain Temp. Coeff.: 5ppm/C
2. Input Res. Temp. Coeff.: -300ppm/C
Answer
Provided that the Vref is a low impedance source, the effect of the absolute
change in i/p resistance will not affect the gain tempco of the device.
Therefore you should use a low impedance ref source and use the gain
temp.co-eff of 5ppm/degC as your reference.