Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Precision DACs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Precision DACs
  • Data Converters
Precision DACs
Documents Can I mix bipolar and unipolar ADCs in a MAX11300 PIXI configuration?
  • Q&A
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +AD3552R: FAQ
  • +AD420: FAQ
  • +AD421: FAQ
  • +AD5024: FAQ
  • +AD5060: FAQ
  • +AD5065: FAQ
  • +AD5115: FAQ
  • +AD5116: FAQ
  • +AD511: FAQ
  • +AD5121: FAQ
  • +AD5141: FAQ
  • +AD5142: FAQ
  • +AD5160: FAQ
  • +AD5161: FAQ
  • +AD5203: FAQ
  • +AD5206: FAQ
  • +AD5222: FAQ
  • +AD5232: FAQ
  • +AD5235: FAQ
  • +AD5243: FAQ
  • +AD5245: FAQ
  • +AD5248: FAQ
  • +AD524: FAQ
  • +AD5251: FAQ
  • +AD5252: FAQ
  • +AD5254: FAQ
  • +AD5258: FAQ
  • +AD5259: FAQ
  • +AD5263: FAQ
  • +AD5270: FAQ
  • +AD5271: FAQ
  • +AD5272: FAQ
  • +AD527x: FAQ
  • +AD5290: FAQ
  • +AD5292: FAQ
  • +AD5293: FAQ
  • +AD5301: FAQ
  • +AD5318: FAQ
  • +AD5321: FAQ
  • +AD5323: FAQ
  • +AD5325: FAQ
  • +AD5331: FAQ
  • +AD5338: FAQ
  • +AD53500: FAQ
  • +AD5363: FAQ
  • +AD536x: FAQ
  • +AD5370: FAQ
  • +AD5383: FAQ
  • +AD5384: FAQ
  • +AD5405: FAQ
  • +AD5412: FAQ
  • +AD5413: FAQ
  • +AD5420: FAQ
  • +AD5421: FAQ
  • +AD5422: FAQ
  • +AD5429: FAQ
  • +AD5439: FAQ
  • +AD5440: FAQ
  • +AD5443: FAQ
  • +AD5446: FAQ
  • +AD5449: FAQ
  • +AD548B: FAQ
  • +AD549: FAQ
  • +AD5522: FAQ
  • +AD5544: FAQ
  • AD5546: FAQ
  • +AD5553: FAQ
  • +AD5554: FAQ
  • +AD5556: FAQ
  • +AD557: FAQ
  • +AD5592R: FAQ
  • +AD5593R: FAQ
  • +AD5623R: FAQ
  • +AD5627: FAQ
  • +AD5640: FAQ
  • +AD565A: FAQ
  • +AD5660: FAQ
  • +AD5662: FAQ
  • +AD5664: FAQ
  • +AD5668: FAQ
  • +AD5669R: FAQ
  • +AD5696R: FAQ
  • +AD5700: FAQ
  • +AD5722R: FAQ
  • +AD5724: FAQ
  • +AD574: FAQ
  • +AD5750: FAQ
  • +AD5755: FAQ
  • +AD5761: FAQ
  • +AD5764: FAQ
  • +AD5780: FAQ
  • +AD5791: FAQ
  • ad667: FAQ
  • +AD674: FAQ
  • +AD688: FAQ
  • +AD693: FAQ
  • +AD694: FAQ
  • +AD698: FAQ
  • +AD8403: FAQ
  • +AD8842: FAQ
  • +AD9913: FAQ
  • +ADG506ATE: FAQ
  • +DAC Communication Troubleshooting: FAQ
  • +DAC Daisy Chain: FAQ
  • +DAC Power-up sequence and Biasing: FAQ
  • +DAC SPI: FAQ
  • +DAC8800: FAQ
  • +GENERAL: FAQ
  • +nanoDAC+: FAQ
  • +Precision Technology Learning Modules
  • +AD667: supply voltage
  • +AD1139: FAQ
  • +AD5535B: FAQ
  • +AD5625: FAQ
  • AD5627R: FAQ
  • +AD5667R: FAQ
  • +AD5671R: FAQ
  • +AD5675: FAQ
  • +AD5684R: FAQ
  • +AD5754: FAQ
  • +AD5755-1: FAQ
  • +AD664: FAQ
  • +AD7305: FAQ
  • +AD7398: FAQ
  • +AD7541A: FAQ
  • +AD7547: FAQ
  • +AD7568: FAQ
  • +AD7805: FAQ
  • +AD7808: FAQ
  • +AD7809: FAQ
  • +AD7835: FAQ
  • +ADN8810: FAQ
  • +DAC08: FAQ
  • +DS4404K: FAQ
  • +DS4422N+: FAQ
  • +DS4424N+: FAQ
  • +General Digipot FAQs
  • +LTC2662: FAQ
  • LTC2672-16 FAQ
  • +LTC2688: FAQ
  • MAX11300: FAQ
  • -MAX11300EVKIT#: FAQ
    • Are the MAX11300 PIXI devices volatile or nonvolatile?
    • Can I build a multiplexer with the switches in the MAX11300?
    • Can I cascade the MAX11300 PIXI SPI ports (daisy-chain devices)?
    • Can I have the MAX11300 ports configured as ADCs with different I/O voltage ranges?
    • Can I have the MAX11300 ports configured as DACs with different I/O voltage ranges?
    • Can I implement a filter circuit with MAX11300 PIXI technology?
    • Can I implement an amplifier circuit with MAX11300 PIXI technology?
    • Can I make a DPST or SPDT switch with the MAX11300?
    • Can I make a SPST switch using the MAX11300?
    • Can I mix bipolar and unipolar ADCs in a MAX11300 PIXI configuration?
    • Can I mix bipolar and unipolar DACs in a MAX11300 PIXI configuration?
    • Can I parallel multiple DAC output ports of the MAX11300 to increase current drive capability?
    • Can I select a different voltage reference source for each ADC port of the MAX11300?
    • Can I select a different voltage reference source for each DAC port of the MAX11300?
    • Can I select the same voltage reference source for both ADC and DAC ports in the MAX11300?
    • Can the MAX11300 PIXI technology support current-loop applications (i.e., driving an external current loop)?
    • How do I connect a system with bidirectional 5V signals to a system with 3V signals using the MAX11300?
    • How do I monitor power supplies with MAX11300 PIXI technology?
    • How do I program or configure a PIXI design using the MAX11300?
    • How do I use level translators to interface to LVTTL or CMOS I/Os for the MAX11300?
    • What are the maximum I/O voltages that the MAX11300 PIXI technology supports?
    • What are typical applications for the MAX11300 PIXI technology?
    • What does PIXI mean for the MAX11300 product?
    • What is the advantage of ADC averaging in the MAX11300?
    • What is the benefit of using an external voltage reference source with the MAX11300?
    • What is the maximum sample rate for an ADC in the MAX11300's PIXI technology?
    • What is the maximum update rate for a DAC in a MAX11300 PIXI configuration?
    • What is the propagation delay for the MAX11300 PIXI technology?
    • What prototyping tools does Maxim Integrated provide for the MAX11300?
    • What reference designs are available for the MAX11300?
    • What simulation tools does Maxim Integrated provide for MAX11300 PIXI technology?
    • What voltage should I supply to AVDDIO and AVSSIO on the MAX11300EVKIT?
    • What's the PIXI port input capacitance for MAX11300 when two ports being configured into analog switch mode?
  • +MAX11300GCM+: FAQ
  • +MAX11300GTL+: FAQ
  • +MAX11300PMB1#: FAQ
  • +MAX11301: FAQ
  • MAX11311GTJ+: FAQ
  • +MAX11311GTJ+T: FAQ
  • +MAX5054BATA+: FAQ
  • +MAX5100BEUP: FAQ
  • MAX5113: FAQ
  • +MAX5113GTJ+: FAQ
  • +MAX5116: FAQ
  • +MAX5141: FAQ
  • MAX5214: FAQ
  • +MAX5214GUA+: FAQ
  • +MAX5215GUA+T: FAQ
  • +MAX5216: FAQ
  • +MAX5217: FAQ
  • +MAX5235AEUB+: FAQ
  • +MAX5259EEE+: FAQ
  • +MAX526CCNG+: FAQ
  • +MAX528CAG+: FAQ
  • +MAX5304: FAQ
  • +MAX5322: FAQ
  • +MAX543: FAQ
  • +MAX5525ETC+: FAQ
  • +MAX5533: FAQ
  • +MAX5541: FAQ
  • +MAX5550: FAQ
  • +MAX5705: FAQ
  • +MAX5715AAUD+: FAQ
  • MAX5719: FAQ
  • +MAX5719AGSD+: FAQ
  • +MAX5725AWP+: FAQ
  • MAX5774: FAQ
  • +MAX5774UCB+D: FAQ
  • +MAX5802BATB+T: FAQ

Can I mix bipolar and unipolar ADCs in a MAX11300 PIXI configuration?

Revision Creation Date Revision Author
Current Revision 10 Feb 2026 2:37 PM EngineerZone
Revision #7 10 Feb 2026 1:23 PM MSDAPI
Revision #6 10 Feb 2026 1:23 PM MSDAPI
Revision #5 19 Dec 2023 1:56 PM MSDAPI
Revision #4 19 Dec 2023 10:00 AM MSDAPI
Revision #3 6 Dec 2023 12:05 PM MSDAPI
Revision #2 6 Dec 2023 10:23 AM MSDAPI
Revision #1 20 Jun 2018 4:03 AM MSDAPI
  • Compare Versions View current version