Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Calibration Implementation Techniques for Multichannel Phased Array Subsystems

    Learn about phase-calibration techniques used for characterizing a 16 transmit and 16 receive X-band phased array subsystem based on a mixed-signal front...

EngineerZone
EngineerZone
Precision DACs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Precision DACs
  • Data Converters
Precision DACs
Documents Can I implement a filter circuit with MAX11300 PIXI technology?
  • Q&A
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +AD3552R: FAQ
  • +AD420: FAQ
  • +AD421: FAQ
  • +AD5024: FAQ
  • +AD5060: FAQ
  • +AD5065: FAQ
  • +AD5115: FAQ
  • +AD5116: FAQ
  • +AD511: FAQ
  • +AD5121: FAQ
  • +AD5141: FAQ
  • +AD5142: FAQ
  • +AD5160: FAQ
  • +AD5161: FAQ
  • +AD5203: FAQ
  • +AD5206: FAQ
  • +AD5222: FAQ
  • +AD5232: FAQ
  • +AD5235: FAQ
  • +AD5243: FAQ
  • +AD5245: FAQ
  • +AD5248: FAQ
  • +AD524: FAQ
  • +AD5251: FAQ
  • +AD5252: FAQ
  • +AD5254: FAQ
  • +AD5258: FAQ
  • +AD5259: FAQ
  • +AD5263: FAQ
  • +AD5270: FAQ
  • +AD5271: FAQ
  • +AD5272: FAQ
  • +AD527x: FAQ
  • +AD5290: FAQ
  • +AD5292: FAQ
  • +AD5293: FAQ
  • +AD5301: FAQ
  • +AD5318: FAQ
  • +AD5321: FAQ
  • +AD5323: FAQ
  • +AD5325: FAQ
  • +AD5331: FAQ
  • +AD5338: FAQ
  • +AD53500: FAQ
  • +AD5363: FAQ
  • +AD536x: FAQ
  • +AD5370: FAQ
  • +AD5383: FAQ
  • +AD5384: FAQ
  • +AD5405: FAQ
  • +AD5412: FAQ
  • +AD5413: FAQ
  • +AD5420: FAQ
  • +AD5421: FAQ
  • +AD5422: FAQ
  • +AD5429: FAQ
  • +AD5439: FAQ
  • +AD5440: FAQ
  • +AD5443: FAQ
  • +AD5446: FAQ
  • +AD5449: FAQ
  • +AD548B: FAQ
  • +AD549: FAQ
  • +AD5522: FAQ
  • +AD5544: FAQ
  • AD5546: FAQ
  • +AD5553: FAQ
  • +AD5554: FAQ
  • +AD5556: FAQ
  • +AD557: FAQ
  • +AD5592R: FAQ
  • +AD5593R: FAQ
  • +AD5623R: FAQ
  • +AD5627: FAQ
  • +AD5640: FAQ
  • +AD565A: FAQ
  • +AD5660: FAQ
  • +AD5662: FAQ
  • +AD5664: FAQ
  • +AD5668: FAQ
  • +AD5669R: FAQ
  • +AD5696R: FAQ
  • +AD5700: FAQ
  • +AD5722R: FAQ
  • +AD5724: FAQ
  • +AD574: FAQ
  • +AD5750: FAQ
  • +AD5755: FAQ
  • +AD5761: FAQ
  • +AD5764: FAQ
  • +AD5780: FAQ
  • +AD5791: FAQ
  • ad667: FAQ
  • +AD674: FAQ
  • +AD688: FAQ
  • +AD693: FAQ
  • +AD694: FAQ
  • +AD698: FAQ
  • +AD8403: FAQ
  • +AD8842: FAQ
  • +AD9913: FAQ
  • +ADG506ATE: FAQ
  • +DAC Communication Troubleshooting: FAQ
  • +DAC Daisy Chain: FAQ
  • +DAC Power-up sequence and Biasing: FAQ
  • +DAC SPI: FAQ
  • +DAC8800: FAQ
  • +GENERAL: FAQ
  • +nanoDAC+: FAQ
  • +Precision Technology Learning Modules
  • +AD667: supply voltage
  • +AD1139: FAQ
  • +AD5535B: FAQ
  • +AD5625: FAQ
  • AD5627R: FAQ
  • +AD5667R: FAQ
  • +AD5671R: FAQ
  • +AD5675: FAQ
  • +AD5684R: FAQ
  • +AD5754: FAQ
  • +AD5755-1: FAQ
  • +AD664: FAQ
  • +AD7305: FAQ
  • +AD7398: FAQ
  • +AD7541A: FAQ
  • +AD7547: FAQ
  • +AD7568: FAQ
  • +AD7805: FAQ
  • +AD7808: FAQ
  • +AD7809: FAQ
  • +AD7835: FAQ
  • +ADN8810: FAQ
  • +DAC08: FAQ
  • +DS4404K: FAQ
  • +DS4422N+: FAQ
  • +DS4424N+: FAQ
  • +General Digipot FAQs
  • +LTC2662: FAQ
  • LTC2672-16 FAQ
  • +LTC2688: FAQ
  • MAX11300: FAQ
  • -MAX11300EVKIT#: FAQ
    • Are the MAX11300 PIXI devices volatile or nonvolatile?
    • Can I build a multiplexer with the switches in the MAX11300?
    • Can I cascade the MAX11300 PIXI SPI ports (daisy-chain devices)?
    • Can I have the MAX11300 ports configured as ADCs with different I/O voltage ranges?
    • Can I have the MAX11300 ports configured as DACs with different I/O voltage ranges?
    • Can I implement a filter circuit with MAX11300 PIXI technology?
    • Can I implement an amplifier circuit with MAX11300 PIXI technology?
    • Can I make a DPST or SPDT switch with the MAX11300?
    • Can I make a SPST switch using the MAX11300?
    • Can I mix bipolar and unipolar ADCs in a MAX11300 PIXI configuration?
    • Can I mix bipolar and unipolar DACs in a MAX11300 PIXI configuration?
    • Can I parallel multiple DAC output ports of the MAX11300 to increase current drive capability?
    • Can I select a different voltage reference source for each ADC port of the MAX11300?
    • Can I select a different voltage reference source for each DAC port of the MAX11300?
    • Can I select the same voltage reference source for both ADC and DAC ports in the MAX11300?
    • Can the MAX11300 PIXI technology support current-loop applications (i.e., driving an external current loop)?
    • How do I connect a system with bidirectional 5V signals to a system with 3V signals using the MAX11300?
    • How do I monitor power supplies with MAX11300 PIXI technology?
    • How do I program or configure a PIXI design using the MAX11300?
    • How do I use level translators to interface to LVTTL or CMOS I/Os for the MAX11300?
    • What are the maximum I/O voltages that the MAX11300 PIXI technology supports?
    • What are typical applications for the MAX11300 PIXI technology?
    • What does PIXI mean for the MAX11300 product?
    • What is the advantage of ADC averaging in the MAX11300?
    • What is the benefit of using an external voltage reference source with the MAX11300?
    • What is the maximum sample rate for an ADC in the MAX11300's PIXI technology?
    • What is the maximum update rate for a DAC in a MAX11300 PIXI configuration?
    • What is the propagation delay for the MAX11300 PIXI technology?
    • What prototyping tools does Maxim Integrated provide for the MAX11300?
    • What reference designs are available for the MAX11300?
    • What simulation tools does Maxim Integrated provide for MAX11300 PIXI technology?
    • What voltage should I supply to AVDDIO and AVSSIO on the MAX11300EVKIT?
    • What's the PIXI port input capacitance for MAX11300 when two ports being configured into analog switch mode?
  • +MAX11300GCM+: FAQ
  • +MAX11300GTL+: FAQ
  • +MAX11300PMB1#: FAQ
  • +MAX11301: FAQ
  • MAX11311GTJ+: FAQ
  • +MAX11311GTJ+T: FAQ
  • +MAX5054BATA+: FAQ
  • +MAX5100BEUP: FAQ
  • MAX5113: FAQ
  • +MAX5113GTJ+: FAQ
  • +MAX5116: FAQ
  • +MAX5141: FAQ
  • MAX5214: FAQ
  • +MAX5214GUA+: FAQ
  • +MAX5215GUA+T: FAQ
  • +MAX5216: FAQ
  • +MAX5217: FAQ
  • +MAX5235AEUB+: FAQ
  • +MAX5259EEE+: FAQ
  • +MAX526CCNG+: FAQ
  • +MAX528CAG+: FAQ
  • +MAX5304: FAQ
  • +MAX5322: FAQ
  • +MAX543: FAQ
  • +MAX5525ETC+: FAQ
  • +MAX5533: FAQ
  • +MAX5541: FAQ
  • +MAX5550: FAQ
  • +MAX5705: FAQ
  • +MAX5715AAUD+: FAQ
  • MAX5719: FAQ
  • +MAX5719AGSD+: FAQ
  • +MAX5725AWP+: FAQ
  • MAX5774: FAQ
  • +MAX5774UCB+D: FAQ
  • +MAX5802BATB+T: FAQ

Can I implement a filter circuit with MAX11300 PIXI technology?

There are no amplifiers in PIXI technology so it is not possible to implement an active filter.
  • A/D and D/A Converter Combinations
  • MAX11300
  • data converters
  • 000094844
  • Mixed-Signal Front Ends (MxFE)
  • Share
  • History
  • More
  • Cancel
Related
Recommended