Hello!
I have a Problem with the AD5627R. (in MSOP Package)
The Output is not Rising higher than 0,3V (@ 0x0FFF), When I change the Input the Output follows so I can see it works somehow.
I am using the internal reference ( I have 2,42V on the reference pin) but I also tried to switch it off and use an external 2,5V reference. In this Case my maximal Output is 0,15V
I also tried to change the supply Voltage from 3V3 to 5V, but nothing changes.
I Pulled the LDAC to Low and CLR to High,
For Initialisation I set the Internal Reference :On and the Power Down Mode: Normal Mode.
I write every 50ms one Channel
Also I Can see on my Logic Analyzer that the Conversation is good.
Anyone a Idea, it will be very helpfull.
Thanks..
Martin