Post Go back to editing

Linear Gain Setting Mode settable by EEPROM

Thread Summary

The user inquired if the AD5143 can be programmed to enter linear gain setting mode after power-up without I2C commands. The final answer confirms that the AD5143 reverts to potentiometer mode after reset or power-up, and it is not possible to set it to linear gain mode without I2C commands.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD5143

I plan to use the AD5143 to set gain of an amplifier during production.In normal operation I2C is not used.

One thing not completely clear to me: is it possible to programm the chip so that linear gain setting mode is active after power up without I2C commands?
I assume that this is not possible because the datasheet states "The devices restore in potentiometer mode after a reset or power-up".
Is this assumption correct?

Regards Christian

Parents Reply Children
No Data
More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.