Post Go back to editing

parameter values

Category: Datasheet/Specs
Product Number: LTC2621

Hello, I am trying to do an accuracy analysis on this part and I was wondering if the following can be provided: 

  1. Offset Error Drift
  2. Reference Temperature Coefficient (TC)
  3. The tolerance on the Vref of Vcc=5V

Thread Notes

Parents
  • Hi  ,

    1. Offset Error Drift
    -> The datasheet doesn't exactly provide the offset drift but if it can suffice your analysis, the Offset Error and Temperature coefficient are available.
    2. Reference Temperature Coefficient
    -> The LTC2621 only uses external reference so this spec will depend on the reference used.
    3. 
    The tolerance on the Vref of Vcc=5V
    -> You can safely use Vref in this range: 0V ≤ VREF ≤ VCC. The tolerance will depend on the stability of the rail and reference used as both of these are external supplies.

    Hope this helps.

    Regards,
    Flynn

Reply
  • Hi  ,

    1. Offset Error Drift
    -> The datasheet doesn't exactly provide the offset drift but if it can suffice your analysis, the Offset Error and Temperature coefficient are available.
    2. Reference Temperature Coefficient
    -> The LTC2621 only uses external reference so this spec will depend on the reference used.
    3. 
    The tolerance on the Vref of Vcc=5V
    -> You can safely use Vref in this range: 0V ≤ VREF ≤ VCC. The tolerance will depend on the stability of the rail and reference used as both of these are external supplies.

    Hope this helps.

    Regards,
    Flynn

Children
No Data