Post Go back to editing

AD5292 wiper not responding when controlled by Raspberry Pi 4(always 1.6V)

Thread Summary

The user is troubleshooting an issue with the AD5292 wiper not moving when connected to a Raspberry Pi 4. The final response acknowledges the issue and promises to review the provided connections and Python test code to provide further assistance. The AD5292 is configured with a 10 kΩ pull-up to 3.3 V on RESET, VLOGIC, and RDY pins, and the SPI interface is connected to GPIO pins 10, 11, 13, and 27.
AI Generated Content
Category: Hardware
Product Number: AD5292

I followed the AD5292 datasheet and also the review from the CCS forum page linked above.
I connected the AD5292 to a Raspberry Pi 4 and ran a simple Python script to test the wiper,
but the wiper does not move anymore.

CCS :: View topic - For anyone who chooses to use the AD5292 in a new design...

Here are my current connections:

1. RESET: 10 kΩ pull‑up to 3.3 V and connected to GPIO17 (Raspberry Pi pin 11)
2. VSS: –15 V
3. A: 3.3 V
4. W: output measurement pin
5. B: GND
6. VDD: +15 V
7. EXT_CAP: 1 µF to GND
8. VLOGIC: 10 kΩ pull‑up to 3.3 V
9. GND
10. DIN: GPIO10 (MOSI) (pin 19)
11. SCLK: GPIO11 (SCLK) (pin 23)
12. SYNC: GPIO8 (CE0) (pin 25)
13. SDO: GPIO9 (MISO) (pin 21)
14. RDY: 10 kΩ pull‑up to 3.3 V and connected to GPIO27 (pin 13)

I also attached my Python test code.
Could someone help me figure out why the wiper is not moving?
Thank you in advance.

ad5292_test.zip

Parents Reply Children
No Data