Category: Hardware
Product Number: LTC2664
Hi
In the schematic the MSP0,1,2 Pins are connected to 5V-0V-0V, which represents a configuration of +/-5V o/p range with mid-scale Reset Code.
Now based on the application change, we would like to change the o/p range to 0V to 5V with Zero-scale reset code.
Can this be done without changing (through rework) the HW setting of the MSP0,1,2 Pins at the board?
I am trying to understand whether the the Hard wired MSPN setting be overwritten by the Software? if so how?
I think driving the CLR/ would help to get the scale as per the reset code given in Table:4 in that particular MSPAN setting and this is not to change the MSPAN setting?
Looking forward some clarity here on this need.
Regards,
Felix.