Post Go back to editing

More precise equivalent pin to pin compatible to AD5663RBRMZ-3

Category: Hardware
Product Number: AD5663RBRMZ-3

Hi

We have selected a Dac AD5663RBRMZ-3 ( 10 lead MSOP package ) 

The data sheet  gives 10mV  max for the offset error and  1.5 % max for the gain error, see below

Performances  like the AD5689/AD5687 , 1.5 mV offset max error and 0.1% max full scale error  shall be more  suitable for our application . Does  there exist an equivalent a pin to pin compatible dac to AD5663RBRMZ-3 ( 10 lead MSOP package )   with these characteristics ?

Thank you for your help .

Best Regards

Aldo

Parents Reply Children
No Data
More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.