Post Go back to editing

More precise equivalent pin to pin compatible to AD5663RBRMZ-3

Category: Hardware
Product Number: AD5663RBRMZ-3

Hi

We have selected a Dac AD5663RBRMZ-3 ( 10 lead MSOP package ) 

The data sheet  gives 10mV  max for the offset error and  1.5 % max for the gain error, see below

Performances  like the AD5689/AD5687 , 1.5 mV offset max error and 0.1% max full scale error  shall be more  suitable for our application . Does  there exist an equivalent a pin to pin compatible dac to AD5663RBRMZ-3 ( 10 lead MSOP package )   with these characteristics ?

Thank you for your help .

Best Regards

Aldo