Post Go back to editing

Supply Voltage Requirements

Thread Summary

The user asked if the AD5263 can be powered from a 5V supply and if the POT pins can use voltages close to the rails. The final answer confirms that the AD5263 can operate with a 5V single supply (VDD = 5V, VSS = 0V) and that the POT pins can use voltages from VSS to VDD, as specified in the Electrical Characteristics section.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD5263

At the top of the AD5263 datasheet, it says it supports 10V to 15V single supply.

In the Electrical Characteristics section of the AD5263 datasheet, however, it says it supports 4.5V to 16.5V.

Can I power it from a single 5V supply and use voltages at the POT pins that go close to the rails?

More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.