Post Go back to editing

AD5328 stops converting after some time problem

Thread Summary

The user experienced an issue where the AD5328ARUZ DAC stopped responding to SPI commands from the MCU, even after rebooting the MCU. The problem was resolved by installing 100pf capacitors between all data lines and ground. The user also noted that the issue could be temporarily resolved by restarting the AD5328ARUZ power supply.
AI Generated Content
Category: Hardware
Product Number: AD5328

I have exactly the same problem. After a while, the chip simply stops executing SPI commands from the MCU. Vdd = 3.3V , Vref a_h = 3.0V

|The ADC stops responding to any commands from the MCU. This applies to both the RESET and the output level settings. Rebooting the MCU does not produce any results. However, the issue can be resolved by restarting the AD5328ARUZ power supply.

Here is an example of how the microcontroller sets the output levels. The SPI frequency is low.

Edit Notes

fix
[edited by: ozoni at 2:44 PM (GMT -5) on 19 Dec 2025]
Parents Reply Children
No Data
More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.